This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678: Hyperlink Errata

Expert 1780 points

Part Number: TMDSEVM6678

Hello,

    We are planning to get two of the TMDSEVM6678 EVMs to test the Hyperlink interface. However the errata of the EVM states that there is a mistake in the beta1 and beta2 versions of the board and the link cannot be used. 

I am unable to decipher the following:

1) What is the version of the board currently being sold?

2) Is the issue fixed? 

3) If not then please advise on how can the interface be tested?

4) Does the board come with code for the interface? 

Regards,