This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2HG: Uart driver can't receive data

Part Number: TDA2HG


Hi,

software version: ti_vision_sdk_v3.5

I just switching the uart2 driver from m4 core to A15. My m4 uart2 driver is fine, pls refer code below.

#include "apa_uart_drv.h"

#include <ti/csl/hw_types.h>
#include <ti/csl/soc.h>

#include <ti/csl/cslr_synctimer.h>
#include <ti/csl/src/ip/uart/V1/hw_uart.h>
#include <ti/csl/src/ip/uart/V1/uart.h>

#include <ti/csl/csl_uart.h>
#include <ti/csl/arch/csl_arch.h>
#include <ti/drv/vps/include/common/bsp_utils.h>
#include <ti/drv/stw_lld/platform/irq_xbar_interrupt_ids.h>
#include <ti/sysbios/family/shared/vayu/IntXbar.h>
#include <src/rtos/utils_common/include/utils.h>

#include "include/link_api/system.h"
#include "include/link_api/system_common.h"
//#include <ti/csl/example/utils/uart_console/inc/uartConfig.h>

extern Int32 Vps_printf(const char *format, ...);

/******************************************************************************
**              INTERNAL MACRO DEFINITIONS
******************************************************************************/
#define XBAR_CPU                        (CSL_XBAR_IRQ_CPU_ID_IPU2)
#if defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_TDA2EX)
//#define UART_INT_ID                     (44U)
//#define XBAR_INST                       (CSL_XBAR_INST_IPU2_IRQ_44)
//#define XBAR_INTR_SOURCE                (CSL_XBAR_UART5_IRQ)
#elif defined (SOC_TDA3XX)
#define UART_INT_ID                     (45U)
#define XBAR_INST                       (CSL_XBAR_INST_IPU1_IRQ_45)
#define XBAR_INTR_SOURCE                (CSL_XBAR_UART3_IRQ)
#endif
//#define UART5_INTR_NUM					68
//#define UART5_INTR_NUM					CSL_XBAR_INST_IPU1_IRQ_45
//#define UART5_INTR_NUM					CSL_XBAR_INST_IPU2_IRQ_69
//#define UART5_INTR_SRC					CSL_XBAR_UART5_IRQ
#define UART2_INTR_NUM					CSL_XBAR_INST_IPU2_IRQ_69
#define UART2_INTR_SRC					CSL_XBAR_UART2_IRQ

/******************************************************************************
**              INTERNAL FUNCTION PROTOTYPES
******************************************************************************/
static void APA_UART_setPinmuxRegs(uint32_t baseAddrOffset, uint32_t ioPinCfg);
static void APA_UART_InstInit(void);
static void APA_UART_IntEnable(uint32_t base);
static void APA_UART_INTCConfig(void);
static void APA_UART_FIFOConfigure(uint32_t base);

static void APA_UART_BaudRateSet(uint32_t base);
/******************************************************************************
**              GLOBAL VARIABLE DEFINITIONS
******************************************************************************/
const uint32_t ruw_apaUartBasePtrs[APA_SOC_MCU_UART_TOTAL] = APA_SOC_MCU_UART_BASE_PTRS;
const APA_SOC_MCU_uart_t rs_apaSocMcuUart[APA_SOC_MCU_UART_TOTAL] = APA_SOC_MCU_UART_INFO;
uint32_t ruw_apaSocMcuUartBase;

BspOsal_IntrHandle gUtils_tempHwiHandle;

/******************************************************************************
**              FUNCTION DEFINITIONS
******************************************************************************/
static void APA_UART_setPinmuxRegs(uint32_t baseAddrOffset, uint32_t ioPinCfg)
{
  uint32_t tmpRegVal;

  /* Unlock MMR_5 for pin muxing */
  HW_WR_REG32(
    SOC_CTRL_MODULE_CORE_CORE_REGISTERS_BASE +
    CTRL_CORE_MMR_LOCK_5,
    CTRL_CORE_MMR_LOCK_5_MMR_LOCK_5_TOUNLOCK);

  tmpRegVal = HW_RD_REG32(SOC_CORE_PAD_IO_REGISTERS_BASE + baseAddrOffset);

  tmpRegVal &= ~(0xF000FU);
  tmpRegVal |= (ioPinCfg & 0xF000FU);

  HW_WR_REG32((SOC_CORE_PAD_IO_REGISTERS_BASE + baseAddrOffset), tmpRegVal);

  /* Lock MMR_5 for pin muxing */
  HW_WR_REG32(
    SOC_CTRL_MODULE_CORE_CORE_REGISTERS_BASE +
    CTRL_CORE_MMR_LOCK_5,
    CTRL_CORE_MMR_LOCK_5_MMR_LOCK_5_TOLOCK);
  return;
}

static void APA_UART_DRV_Pinmux_Init(void)
{
  uint8_t cnt;
  const APA_SOC_MCU_uart_t* pUart = rs_apaSocMcuUart;

  for(cnt = 1u; cnt < APA_SOC_MCU_UART_TOTAL; cnt ++)
  {
    /*Pad configuration and PRCM enable*/
    APA_UART_setPinmuxRegs((pUart + cnt)->rxdPadBaseOffset, (pUart + cnt)->rxdMuxVal);
    APA_UART_setPinmuxRegs((pUart + cnt)->txdPadBaseOffset, (pUart + cnt)->txdMuxVal);
  }
}

static void APA_UART_InstInit(void)
{
  ruw_apaSocMcuUartBase = ruw_apaUartBasePtrs[APA_SOC_MCU_UART_INST_1];
}

/*
** A wrapper function performing FIFO configurations.
*/
static void APA_UART_FIFOConfigure(uint32_t base)
{
  uint32_t fifoConfig = 0;

  /* Setting the TX and RX FIFO Trigger levels as 1. No DMA enabled. */
  fifoConfig = UART_FIFO_CONFIG(UART_TRIG_LVL_GRANULARITY_1,
                                UART_TRIG_LVL_GRANULARITY_4,
                                1,
                                UART_FCR_RX_TRIG_LVL_60,
                                1,
                                1,
                                UART_DMA_EN_PATH_SCR,
                                UART_DMA_MODE_0_ENABLE);

  /* Configuring the FIFO settings. */
  UARTFIFOConfig(base, fifoConfig);
}

/*
** A wrapper function performing Baud Rate settings.
*/

static void APA_UART_BaudRateSet(uint32_t base)
{
  uint32_t divisorValue = 0;

  /* Computing the Divisor Value. */
  divisorValue = UARTDivisorValCompute(APA_SOC_MCU_UART_MODULE_CLK,
                                       APA_SOC_MCU_UART_BR_230400,
                                       UART16x_OPER_MODE,
                                       UART_MIR_OVERSAMPLING_RATE_42);

  /* Programming the Divisor Latches. */
  UARTDivisorLatchWrite(base, divisorValue);
}

/*
** A wrapper function performing Interrupt configurations.
*/
static void APA_UART_IntEnable(uint32_t base)
{
  /* Configuring INTC to receive UART interrupts. */
  APA_UART_INTCConfig();
  /* Enabling the specified UART interrupts. */
  UARTIntEnable(base, UART_INT_RHR_CTI);
}

/*
** This function configures the INTC to receive UART interrupts.
*/
static void APA_UART_INTCConfig(void)
{
#if 0
  /* Crossbar registers are already unlocked, so connect directly */
  CSL_xbarIrqConfigure(XBAR_CPU,XBAR_INST,XBAR_INTR_SOURCE);

  /* Initializing the Interrupt Controller. */
  Intc_Init();

  /* Enable the interrupt */
  Intc_IntEnable(0);

  /* Registering the Interrupt Service Routine(ISR). */
  Intc_IntRegister(UART_INT_ID, (IntrFuncPtr) APA_UART_Isr, NULL);

  /* Setting the priority for the UART interrupt in INTC. */
  Intc_IntPrioritySet(UART_INT_ID, 1, 0);

  /* Enabling the UART interrupt in INTC. */
  Intc_SystemEnable(UART_INT_ID);
#else
  UInt32 cookie = 0;
  Vps_printf(" UTILS: IntXbar_connectIRQT !!!\n");
  //IntXbar_connectIRQ(UART5_INTR_NUM, XBAR_INTR_SOURCE);

  IntXbar_connectIRQ(UART2_INTR_NUM, UART2_INTR_SRC);
  //BspOsal_irqXbarConnect(UART5_INTR_NUM, CSL_XBAR_UART5_IRQ);
  //BspOsal_irqXbarConnectIrq(UART5_INTR_NUM, UART5_INTR_SRC);
  /* Disabling the global interrupts */
  cookie = Hwi_disable();

  Vps_printf(" UTILS: UART2 INTERRUPT: HWI Create for INT%d !!!\n", UART2_INTR_NUM);

  gUtils_tempHwiHandle = BspOsal_registerIntr(UART2_INTR_NUM,
                         (BspOsal_IntrFuncPtr)APA_UART_Isr,
                         NULL
                                             );

  if( gUtils_tempHwiHandle == NULL)
  {
    Vps_printf(" UTILS: UART2 INTERRUPT: HWI Create Failed !!!\n");
    UTILS_assert(0);
  }
  Vps_printf(" UTILS: Hwi_enableInterrupt !!!\n");
  /* Enable the interrupt */
  Hwi_enableInterrupt(UART2_INTR_NUM);
  Vps_printf(" UTILS: Hwi_restore !!!\n");
  /* Restore interrupts */
  Hwi_restore(cookie);

#endif
}


void APA_UART_Init(void)
{
  APA_UART_InstInit();

  //APA_UART_DRV_Pinmux_Init();

  /* Performing a module reset. */
  UARTModuleReset(ruw_apaSocMcuUartBase);

  /* Performing FIFO configurations. */
  APA_UART_FIFOConfigure(ruw_apaSocMcuUartBase);

  /* Performing Baud Rate settings. */
  APA_UART_BaudRateSet(ruw_apaSocMcuUartBase);

  /* Switching to Configuration Mode B. */
  UARTRegConfigModeEnable(ruw_apaSocMcuUartBase, UART_REG_CONFIG_MODE_B);

  /* Programming the Line Characteristics. */
  UARTLineCharacConfig(ruw_apaSocMcuUartBase,
                       (UART_FRAME_WORD_LENGTH_8 | UART_FRAME_NUM_STB_1),
                       UART_PARITY_NONE);
  /* Disabling write access to Divisor Latches. */
  UARTDivisorLatchDisable(ruw_apaSocMcuUartBase);

  /* Disabling Break Control. */
  UARTBreakCtl(ruw_apaSocMcuUartBase, UART_BREAK_COND_DISABLE);

  /* Switching to UART16x operating mode. */
  UARTOperatingModeSelect(ruw_apaSocMcuUartBase, UART16x_OPER_MODE);

  /* Performing Interrupt configurations. */
  APA_UART_IntEnable(ruw_apaSocMcuUartBase);
}

void IntDisable(void)
{
  /* Clear GIE */
  asm (" CPSID I");
}

void IntEnable(uint32_t status)
{
  asm (" CPSIE I");
}




But after I disabled m4 uart2 driver and enable it on A15 dts file:

// DISABLE_COMPLETE(uart2);

uart2: serial@4806c000 {
	compatible = "ti,dra742-uart", "ti,omap4-uart";
	reg = <0x4806c000 0x100>;
	interrupts = <GIC_SPI 68 IRQ_TYPE_LEVEL_HIGH>;
	ti,hwmods = "uart2";
	clock-frequency = <48000000>;
	status = "disabled";
	dmas = <&edma_xbar 51 0>, <&edma_xbar 52 0>;
	dma-names = "", "";
};

&uart2 {
	status = "okay";
};

dmesg shows below:

[    1.698409] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250

So I think the driver is loaded. But when I use code which is tested ok before, to receive data, it always timeout.

7115.uart.cpp

I checked register "0x4806C000"(UART_RHR), it aways 0. So I think it never received on phy layer.

Since my m4 uart2 driver didn't use dma, so I disable dma in dts, still not work.

I attach A15 driver configured register dump below:

root@dra7xx-evm:~# devmem2 0x4806C000
/dev/mem opened.
Memory mapped at address 0xb6f7b000.
Read at address  0x4806C000 (0xb6f7b000): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C004
/dev/mem opened.
Memory mapped at address 0xb6fd9000.
Read at address  0x4806C004 (0xb6fd9004): 0x00000005
root@dra7xx-evm:~# devmem2 0x4806C008
/dev/mem opened.
Memory mapped at address 0xb6fc4000.
Read at address  0x4806C008 (0xb6fc4008): 0x000000C1
root@dra7xx-evm:~# devmem2 0x4806C00c
/dev/mem opened.
Memory mapped at address 0xb6fde000.
Read at address  0x4806C00C (0xb6fde00c): 0x00000013
root@dra7xx-evm:~# devmem2 0x4806C010
/dev/mem opened.
Memory mapped at address 0xb6f47000.
Read at address  0x4806C010 (0xb6f47010): 0x00000003
root@dra7xx-evm:~# devmem2 0x4806C014
/dev/mem opened.
Memory mapped at address 0xb6f34000.
Read at address  0x4806C014 (0xb6f34014): 0x00000060
root@dra7xx-evm:~# devmem2 0x4806C018
/dev/mem opened.
Memory mapped at address 0xb6f85000.
Read at address  0x4806C018 (0xb6f85018): 0x00000020
root@dra7xx-evm:~# devmem2 0x4806C01c
/dev/mem opened.
Memory mapped at address 0xb6fb4000.
Read at address  0x4806C01C (0xb6fb401c): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C020
/dev/mem opened.
Memory mapped at address 0xb6f93000.
Read at address  0x4806C020 (0xb6f93020): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C024
/dev/mem opened.
Memory mapped at address 0xb6f06000.
Read at address  0x4806C024 (0xb6f06024): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C028
/dev/mem opened.
Memory mapped at address 0xb6f2f000.
Read at address  0x4806C028 (0xb6f2f028): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C02c
/dev/mem opened.
Memory mapped at address 0xb6f4e000.
Read at address  0x4806C02C (0xb6f4e02c): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C030
/dev/mem opened.
Memory mapped at address 0xb6eff000.
Read at address  0x4806C030 (0xb6eff030): 0x00000042
root@dra7xx-evm:~# devmem2 0x4806C034
/dev/mem opened.
Memory mapped at address 0xb6ff7000.
Read at address  0x4806C034 (0xb6ff7034): 0x00000007
root@dra7xx-evm:~# devmem2 0x4806C038
/dev/mem opened.
Memory mapped at address 0xb6f7a000.
Read at address  0x4806C038 (0xb6f7a038): 0x00000040
root@dra7xx-evm:~# devmem2 0x4806C03c
/dev/mem opened.
Memory mapped at address 0xb6fe5000.
Read at address  0x4806C03C (0xb6fe503c): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C040
/dev/mem opened.
Memory mapped at address 0xb6fef000.
Read at address  0x4806C040 (0xb6fef040): 0x000000C9
root@dra7xx-evm:~# devmem2 0x4806C044
/dev/mem opened.
Memory mapped at address 0xb6fa3000.
Read at address  0x4806C044 (0xb6fa3044): 0x00000004
root@dra7xx-evm:~# devmem2 0x4806C048
/dev/mem opened.
Memory mapped at address 0xb6f48000.
Read at address  0x4806C048 (0xb6f48048): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C050
/dev/mem opened.
Memory mapped at address 0xb6fd6000.
Read at address  0x4806C050 (0xb6fd6050): 0x50412E03
root@dra7xx-evm:~# devmem2 0x4806C054
/dev/mem opened.
Memory mapped at address 0xb6f42000.
Read at address  0x4806C054 (0xb6f42054): 0x0000000D
root@dra7xx-evm:~# devmem2 0x4806C058
/dev/mem opened.
Memory mapped at address 0xb6f6b000.
Read at address  0x4806C058 (0xb6f6b058): 0x00000001
root@dra7xx-evm:~# devmem2 0x4806C05c
/dev/mem opened.
Memory mapped at address 0xb6f40000.
Read at address  0x4806C05C (0xb6f4005c): 0x000000FF
root@dra7xx-evm:~# devmem2 0x4806C060
/dev/mem opened.
Memory mapped at address 0xb6f77000.
Read at address  0x4806C060 (0xb6f77060): 0x00000069
root@dra7xx-evm:~# devmem2 0x4806C064
/dev/mem opened.
Memory mapped at address 0xb6f0b000.
Read at address  0x4806C064 (0xb6f0b064): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C068
/dev/mem opened.
Memory mapped at address 0xb6f1c000.
Read at address  0x4806C068 (0xb6f1c068): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C06c
/dev/mem opened.
Memory mapped at address 0xb6fb0000.
Read at address  0x4806C06C (0xb6fb006c): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C070
/dev/mem opened.
Memory mapped at address 0xb6feb000.
Read at address  0x4806C070 (0xb6feb070): 0x00000003
root@dra7xx-evm:~# devmem2 0x4806C074
/dev/mem opened.
Memory mapped at address 0xb6fa3000.
Read at address  0x4806C074 (0xb6fa3074): 0x0000001A
root@dra7xx-evm:~# devmem2 0x4806C080
/dev/mem opened.
Memory mapped at address 0xb6f22000.
Read at address  0x4806C080 (0xb6f22080): 0x00000000
root@dra7xx-evm:~# devmem2 0x4806C084
/dev/mem opened.
Memory mapped at address 0xb6f26000.
Read at address  0x4806C084 (0xb6f26084): 0x00000000

Would you please tell me what I missed? Thanks!