Part Number: AM3352
Hi,
I have qestions about DDR controller for AM335x. I use SDRAM (DDR3: 800MHz).
Q1: I think the DQS signal needs to be shifted because the DQS and DQ signals are in the same phase at the read timing.
I believe this DQS signal shift is done by the value of RD_DQS_SLAVE_RATIO_CS0, is that correct?
Q2: Is it correct to think that the meaning of RD_DQS_SLAVE_RATIO_CS0 value is the delay time, which is the value of 256 divisions of the period of DDR_CK?
Q3: What is the reason why the reset value of RD_DQS_SLAVE_RATIO_CS0 is 0x40?
Q4: Please tell me about the structure and operation of the master and slave DLLs here.
Q5: Can I assume that the minimum setup time and maximum hold time for the memory controller side (EMIF) are the same as the DDR memory specifications?
Setup time: 75 ps(MIN)
Hold time: 100 ps(max)
Best Regards,
H.U