Hello,
I am using the PSP UART example to communicate with the EVM6747. When I boot up from the emulator or the onboard SPI flash everything works fine. When I bootup from the same UART (using the TI UART boot host) the UART does not respond. I am running at 115kbaud and have not tried any other speeds. Why would booting from the UART stop the uart from working but the SPI flash boot work fine?
In my target hardware I will be booting from the UART hence the need to have this working.
Regards,
Fawad