This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: How can I change MPU clock?

Part Number: TDA2P-ACD


Hello.

The below is my environment.

Chip : TDA2PHFUQACDQ1
SDK : PROCESSOR_SDK_VISION_03_08_00_00
U-Boot : 2019.01
Linux : 4.19.73+

Currently, MPU clock is 1GHz(opp_nom).

---------------
| DPLL_MPU |
---------------
| Locked |
| |
| Lock |
| Auto LPST |
| |
| |
| |
| |
| |
| Disabled |
| |
| Disabled |
| Disabled |
| 2 |
| No Ramp |
| |
| CLKINPULOW |
| 1 |
| Disabled |
| Disabled |
| |
| 20.000 |
| 500 |
| 9 |
| 2000 |
| |
| |
| Enabled |
| 1 (x2) |
| 1000 |
| |

How can I change MPU clock to 1.5GHz(opp_high)?

Best Regards.
Yousik.