Part Number: DRA829V
Tool/software: TI C/C++ Compiler
Hi,
We are trying to configuration for MCU_SPI0 in J7-DRA829
We need to know how to set the baud rate as 1 Mbps.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRA829V
Tool/software: TI C/C++ Compiler
Hi,
We are trying to configuration for MCU_SPI0 in J7-DRA829
We need to know how to set the baud rate as 1 Mbps.
Hi,
Please find the reply below for your queries.
Is that hw unit CSIB0 is mapped to MCU_SPI0?
>> Yes. Please refer mcusw/mcal_drv/docs/drv_docs/modules.html for more details.
How to set 1 Mbps?
>> Please program SpiExtDeviceClockDivider to 47 in the configurator to achieve 1 MHz clock. Please refer SpiExtDeviceClockDivider description in GUI for more details.
Regards,
Sunil Kumar M S
Hi Sunil,
Thanks for your information,
In the EB Tresos Configurator, I did not see more information regarding SpiExtDeviceClockDivider .
May i know How 47 will be relates to 1 MHz.
did you verify the configuration file. ?
we are facing one more issue like, when we change the HW_Unit to 1 - Getting redefined compilation error . May i Know what could be the problem for this parameter ?
Hi Muthushankar,
The value you configure in SpiExtDeviceClockDivider acts as 12 bit clock divider + 1.
SpiExtDeviceClockDivider internally split into 4 bit LSB bit will be programmed to CLKD register and remaining 8 bits to EXTCLK register. Together concatenated acts as 12 bit programmable divider. In the driver, clock granularity is set to 1 clock cycle. Please refer TRM for more details.
By default Spi runs at 48 MHZ.
So 47(0x2F) as a 12 bit divider split into 000000101111 i.e 32 +15 + 1 = 48. (48 MHZ / 48 = 1 MHZ) I hope this answered your question.
Regarding redefined compilation error, please let me know what error you getting?
Regards,
Sunil Kumar M S
Hi Sunil,
Thanks a lot for your detailed information,
shared details are enough for me to proceed further,
For compilation error happen due to below two parameters, if the value as 7 I did not get the error.
But we configured value as 2, i am getting below error.
can you please share some information regarding this.
is this problem with our configuration or those parameter are depends on other parameters?
/**
* \brief Maximum HW unit - This should match the sum for the below units ISR
* which are ON.
*/
#define SPI_MAX_HW_UNIT (7)
/**
* \brief Maximum external device cfg
*/
#define SPI_MAX_EXT_DEV (7)
Compilation error:
error: symbol "Spi_DrvObj" redefined: first defined in "<whole-program>";
redefined in
"/home/user/GCP/psdk_rtos_auto_j7_06_02_00_21/mcusw/binary/mcal/Spi/lib/j721
e/r5f/release/spi.aer5f<Spi.oer5f>"
error: symbol "Spi_DrvStatus" redefined: first defined in "<whole-program>";
redefined in
"/home/user/GCP/psdk_rtos_auto_j7_06_02_00_21/mcusw/binary/mcal/Spi/lib/j721
e/r5f/release/spi.aer5f<Spi.oer5f>"
error: symbol "Spi_getHwUnitBaseAddr" redefined: first defined in
"<whole-program>"; redefined in
"/home/user/GCP/psdk_rtos_auto_j7_06_02_00_21/mcusw/binary/mcal/Spi/lib/j721
e/r5f/release/spi.aer5f<Spi_Priv.oer5f>
Hi Muthushankar,
Please configure via EB Tresos instead of hardcoding it, because there will be dependency on other parameters so.
Regards,
Sunil Kumar M S