This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-DRA8X-TDA4X: LSC Issue

Part Number: PROCESSOR-SDK-DRA8X-TDA4X

Hi, 

I generated LSC gains for IMX390 with input RAW image(1936 x 1086), with M = 64 and N = 64, so I got 576 entries for each channel and 576 * 4 gains in total. I filled the details in "tiovx/kernels_j7/hwa/vpac_viss/vx_vpac_viss_target_dcc.c", in "tivxVpacVissDccMapLscParams" as follows, 

uint32_t grawfe_lsc_tbl[] =
{
#include "lsc_gains.txt"
};

lscCfg->enable = (uint32_t)TRUE;
lscCfg->gainFmt = RFE_LSC_GAIN_FMT_U8Q8_1;
lscCfg->horzDsFactor = RFE_LSC_DS_FACTOR_64;
lscCfg->vertDsFactor = RFE_LSC_DS_FACTOR_64;
lscCfg->tableAddr = grawfe_lsc_tbl;
lscCfg->numTblEntry = 576;

In this above settings I'm seeing only 1/4th of the image was shading corrected. Remaining 3/4th image are not proper.

But for the below settings if I changed the lscCfg->numTblEntry = 2304; (576*4 = 2304), then my image is 100% proper and shading corrected, is this the expected behavior?

lscCfg->enable = (uint32_t)TRUE;
lscCfg->gainFmt = RFE_LSC_GAIN_FMT_U8Q8_1;
lscCfg->horzDsFactor = RFE_LSC_DS_FACTOR_64;
lscCfg->vertDsFactor = RFE_LSC_DS_FACTOR_64;
lscCfg->tableAddr = grawfe_lsc_tbl;
lscCfg->numTblEntry = 2304;