Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Hi,
I'm using the J7 EVM with the PSDKLA/PSDKRA. I was able to run successfully the single_camera out-of-the-box demo, and also connecting another sensor to native CSI interface (instead of the Fusion board), modify the driver and see the video on the monitor.
My questions are as follows:
1. How new camera sensors are enumerated? I saw that the manual defines the method which includes adding a folder, source code file and adding the new sensor in the concerto.mak file. Could you please point me to where in the code and explain how this is performed? All I see that this is performed via RPC command
2. When connecting multiple camera sensors - how does the system know which/how many/where the sensors are connected? How does the application handles the selection between them?
Thanks,
Matan