Part Number: PROCESSOR-SDK-AM335X
Hi,
I have been struggling for some time trying to get the latest Wilink 8 Time Sync support compiled and running on BeagleBoneBlack with the Stream Unlimited multiroom cape. The intention is to get Time Sync running as described in "WL18xx Clock Synchronisation with NTP" for a commercial product.
My first issue is trying to get a recent kernel to compile with the wilink build-utilites. Here is a summary of what I have found so far:
Using build-utilites from here
git clone git://git.ti.com/wilink8-wlan/build-utilites.git
and using the DEFAULT settings in setup-env:
export TOOLCHAIN_PATH=DEFAULT
export KERNEL_PATH=DEFAULT
then ./build_wl18xx.sh update R8.7_SP3 succeeds and makes a 4.1 kernel with drivers that include some of but not all the needed time sync support. However 4.1 is far too old to be secure and we need a more recent kernel.
The TI processor SDK from ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin installs fine, but includes only a 3.1 kernel. Far too old.
The TI processor SDK from ti-processor-sdk-linux-am335x-evm-06.03.00.106-Linux-x86-Install.bin installs fine and builds a 4.19 kernel but it does not include the necessary Time Sync support in the wilink drivers.
So naturally I tried to build build-utilites using the ti-processor-sdk-linux-am335x-evm-06.03.00.10 SDK with setup-env like:
export TOOLCHAIN_PATH=/opt/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/
export KERNEL_PATH=/opt/ti-processor-sdk-linux-am335x-evm-06.03.00.106/board-support/linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85/
But this fails with many compilation errors, due to the fact that kernel 4.19 has many changes incompatible with the wilink and mac80211 drivers in build-utilites, such as changes from init_timer() now not supported to timer_init(). mmc_power_restore_host() and mmc_power_save_host() have been removed
etc etc, including many very low level problem apparently due to errors/omissions in backports etc. I read a comment from Saurabh that this process only works up to kernel 4.4.
So, my main question is: what is the approved way to build a 4.19 (or later) kernel with the time sync support required to do Time Sync between Wilink 8 equipped BBBs?
Supplemantary question. In "WL18xx Clock Synchronisation with NTP" it refers to the procedure to add time sync support using a link to a patch set from
gforge.ti.com/gf/download/user/1160/7841/sdk8-ntp-wilink8-v0.2.tar.gz
this link is no longer valid, but it appears it contained a bunch of patches to add the necessary time sync support to wilink 8 drivers, plus patches to ntp etc. How can I get this patch set?