Part Number: AM5728
Hi all
I have a program.
When I insert USB 3.0 to my am5728.
I can't watch where it mount.
Here is Log:
[ 1886.985995] usb-storage 3-1.2:1.0: USB Mass Storage device detected
[ 1887.012893] scsi host1: usb-storage 3-1.2:1.0
[ 1888.073193] scsi 1:0:0:0: Direct-Access JetFlash Transcend 8GB 1.00 PQ: 0 ANSI: 6
[ 1888.084904] sd 1:0:0:0: [sdb] 15433728 512-byte logical blocks: (7.90 GB/7.36 GiB)
[ 1888.094792] sd 1:0:0:0: [sdb] Write Protect is off
[ 1888.099851] sd 1:0:0:0: [sdb] Write cache: disabled, read cache: disabled, doesn't support DPO or FUA
[ 1888.112181] sdb:
[ 1888.116176] sd 1:0:0:0: [sdb] Attached SCSI removable disk
[ 1888.217268] FAT-fs (sdb): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
Here is Log about usb2.0:
[ 1762.924369] usb-storage 1-1.4:1.0: USB Mass Storage device detected
[ 1762.952965] scsi host0: usb-storage 1-1.4:1.0
[ 1763.993766] scsi 0:0:0:0: Direct-Access SanDisk Cruzer Blade 1.00 PQ: 0 ANSI: 6
[ 1764.005357] sd 0:0:0:0: [sda] 15232000 512-byte logical blocks: (7.80 GB/7.26 GiB)
[ 1764.014643] sd 0:0:0:0: [sda] Write Protect is off
[ 1764.020335] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
[ 1764.040611] sda: sda1
[ 1764.045512] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 1764.354601] FAT-fs (sda1): utf8 is not a recommended IO charset for FAT filesystems, filesystem will be case sensitive!
[ 1764.370351] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
thanks
HY Ken