Hello all,
We are testing QNX+RTOS mode using this SDK 7.0. Please find the logs in the attachment and also dependency packages screenshot.
Regarding Display, we couldn' able to see anything on the screen,
How to debug this issue ?
U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 15:08:08 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Remoteproc 2 started successfully ** File not found /lib/firmware/j7-mcu-r5f0_0-fw ** Starting ATF on ARM64 core... NOTICE: BL31: v2.3():07.00.00.005-dirty NOTICE: BL31: Built : 14:33:55, Jun 17 2020 U-Boot SPL 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000) SYSFW ABI: 3.0 (firmware rev 0x0014 '20.04.1-v2020.04a (Terrific Lla') Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 U-Boot 2020.01-gf9b0d030d3 (Jun 17 2020 - 14:34:25 +0000) SoC: J721E SR1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM1-SOM rev E2 DRAM: 4 GiB not found for dev hbmc-mux Flash: 0 Bytes MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Net: eth0: ethernet@046000000 Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 102 bytes read in 2 ms (49.8 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1513552 bytes read in 36 ms (40.1 MiB/s) Load Remote Processor 6 with data@addr=0x80080000 1513552 bytes: Success! 1513552 bytes read in 36 ms (40.1 MiB/s) Load Remote Processor 7 with data@addr=0x80080000 1513552 bytes: Success! 9314232 bytes read in 197 ms (45.1 MiB/s) Load Remote Processor 8 with data@addr=0x80080000 9314232 bytes: Success! 7653252 bytes read in 162 ms (45.1 MiB/s) ## Starting application at 0x80080000 ... MMU: 16-bit ASID 44-bit PA TCR_EL1=b5183519 cpu0: MPIDR=80000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Display set to R5 Loading IFS...decompressing...done cpu1: MPIDR=80000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 System page at phys:0000000080011000 user:ffffff8040252000 kern:ffffff8040251000 Starting next program at vffffff8060084ae0 MMFLAGS=1 All ClockCycles offsets within tolerance Welcome to QNX Neutrino 7.0 on TI J721E EVM Board!! Starting random service ... start serial driver Starting MMC/SD memory card driver... eMMC Toggle GPIO_uSD_PWR_EN for uSD Starting MMC/SD memory card driver... SD Starting OTG1 controller in the host mode (/dev/usb/*).... Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: S0J56X Rev: 1.0 Setting environment variables... done.. Looking for user script to run: /sd/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Starting shmemallocator.. Starting tiipc-mgr.. Mailbox_plugInterrupt: interrupt Number 489, arg 0x1011EB78 Mailbox_plugInterrupt: interrupt Number 490, arg 0x1011ED10 Mailbox_plugInterrupt: interrupt Number 491, arg 0x1011EEA8 Mailbox_plugInterrupt: interrupt Number 492, arg 0x1011F040 Mailbox_plugInterrupt: interrupt Number 493, arg 0x1011F1D8 Starting TI IPC Resmgr Starting tiudma-mgr.. Start screen.. screen started with dss_on_r5 configuration.. done... J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# s;lo local login logout J7EVM@QNX:/# s;lo lo slog2 slog2info Jan 01 00:00:00.016 random.5 slog* 0 random: Selecting timer as entropy source Jan 01 00:00:00.016 random.5 slog 0 random: All ready, registering path names Jan 01 00:00:00.016 random.5 slog 0 random: Daemonizing the process Jan 01 00:00:00.031 devb_sdmmc_am65x.9 slog* 1800 devb-sdmmc-am65x 1.00A (Jun 26 2020 12:47:18) Jan 01 00:00:00.032 devb_sdmmc_am65x.9 slog 0 libcam.so (Aug 2 2019 15:41:15) bver 606010d Jan 01 00:00:00.033 devb_sdmmc_am65x.9 slog 1800 sdio_cd: insertion path 0, cd state 0x1 Jan 01 00:00:00.056 devb_sdmmc_am65x.49162 slog* 1800 devb-sdmmc-am65x 1.00A (Jun 26 2020 12:47:18) Jan 01 00:00:00.057 devb_sdmmc_am65x.49162 slog 0 libcam.so (Aug 2 2019 15:41:15) bver 606010d Jan 01 00:00:00.058 devb_sdmmc_am65x.49162 slog 1800 sdio_cd: insertion path 0, cd state 0x1 Jan 01 00:00:00.064 io_usb_otg.61451 slog* 0 main(447)[tid:1]: io-usb-otg (Nov 20 2019 16:51:50) args: -d xhci ioport=0x6010000,irq=128,iosize=65536,nousb3 Jan 01 00:00:00.068 io_usb_otg.61451 slog 0 xhci_controller_init(2607): devu-hcd-xhci.so (Nov 20 2019 16:42:36): args nousb3 Jan 01 00:00:00.068 io_usb_otg.61451 slog 8 usb_enum_port(92)[tid:1]: busno 0, parent -1, port 0, High speed Jan 01 00:00:00.068 io_usb_otg.61451 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 8) Jan 01 00:00:00.068 io_usb_otg.61451 slog 12 usb_device_set_address(245)[tid:1]: b:0 devno 0 Jan 01 00:00:00.068 io_usb_otg.61451 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 1, index 0, length 18) Jan 01 00:00:00.068 io_usb_otg.61451 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 9) Jan 01 00:00:00.069 io_usb_otg.61451 slog 11 usb_client_descriptor_get(198)[tid:1]: (type 2, index 0, length 25) Jan 01 00:00:00.069 io_usb_otg.61451 slog 8 usb_enum_port(139)[tid:1]: vid 0x0000, did 0x0000 enumerated(busno 0, devno 0:0) Jan 01 00:00:00.069 io_usb_otg.61451 slog 11 hub_state_inserted(569)[tid:1]: bdentry 0, dentry 0 269635584 Jan 01 00:00:00.069 io_usb_otg.61451 slog 13 hub_configuration_enable(263)[tid:1]: 1 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 MMC CID: Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 MID 0x13, OID 0x4e, PNM S0J56X Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 PRV 0x10, PSN 0x8c64641, MDT 10-2018 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 MMC CSD: Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 CSD_STRUCTURE 3, SPEC_VERS 4, CCC 0x8f5 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 TAAC 127, NSAC 1, TRAN_SPEED 50 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 C_SIZE 4095, C_SIZE_MULT 7 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 ERASE GRP_SIZE 31, GRP_MULT 31, SIZE 0 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 blksz 512, sectors 2097152, dtr 25000000 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 MMC EXT CSD: Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 DEVICE_TYPE 0x57, EXT_CSD_REV 8 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 SEC_COUNT 31080448, dtr 200000000 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 HC_ERASE_GRP_SIZE 1, HC_WP_GRP_SIZE 16 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 STROBE 0x0, BKOPS_EN 0x0 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 Driver type: 0x0 Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 1800 CFG: Timing HS200, DTR 200000000, Bus Width 8 bit Jan 01 00:00:00.124 devb_sdmmc_am65x.9 slog 100 cam-disk.so (Aug 2 2019 15:41:25) Jan 01 00:00:00.171 io_usb_otg.61451 slog 0 usbh_timeout_init(203)[tid:1]: Complete Jan 01 00:00:00.176 io_usb_otg.61451 slog 0 usbh_bus_status_update(309)[tid:1]: busno 0, value = 0 critical error reported Jan 01 00:00:00.176 io_usb_otg.61451 slog 8 usb_enum_port_extract(170)[tid:7]: (busno 0, pdevno 0, portno 1) Jan 01 00:00:00.176 io_usb_otg.61451 slog 8 usb_enum_port_extract(190)[tid:7]: status (2) Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 SD CID: Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 MID 0x3, OID 0x5344, PNM SL16G Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 PRV 0xf4, PSN 0x39f40f90, MDT 3-2019 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 SD CSD: Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 CSD_STRUCTURE 1, SPEC_VERS 0, CCC 0x5b5 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 TAAC 14, NSAC 0, TRAN_SPEED 50 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 C_SIZE 30386, C_SIZE_MULT 0 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 READ_BL_LEN 9, WRITE_BL_LEN 9 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 ERASE GRP_SIZE 0, GRP_MULT 0, SIZE 127 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 blksz 512, sectors 31116288, dtr 25000000 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 SD SW CAPS: Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 bus mode 0x1f, cmd sys 0x1 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 drv type 0xf, curr limit 0xf Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 dtr 50000000 Jan 01 00:00:00.229 devb_sdmmc_am65x.49162 slog 1800 CFG: Timing SDR104, DTR 200000000, Bus Width 4 bit Jan 01 00:00:00.230 devb_sdmmc_am65x.49162 slog 100 cam-disk.so (Aug 2 2019 15:41:25) Jan 01 00:00:00.396 shmemallocator.81934 slog* 0 SharedMemoryAllocator: BaseAddress: 0xae000000 Size: 0x20000000 (536870912) Jan 01 00:00:00.396 shmemallocator.81934 slog 0 SharedMemoryAllocator: BaseAddress: 0x00000000 Size: 0x00000000 (0) Jan 01 00:00:00.583 screen.94225 slog* 300 screen: starting up... Jan 01 00:00:00.585 screen.94225 slog 300 screen: Configuration file: /sd/usr/lib/graphics/jacinto7/graphics.conf.dss_on_r5 Jan 01 00:00:00.593 screen.94225 slog 300 screen: slog2 context created with 1 pages Jan 01 00:00:00.593 screen.94225 slog 300 screen: loading alloc module stdbuf... Jan 01 00:00:00.595 screen.94225 slog 300 screen: display 1 returned invalid value 0 for WFD_PORT_MODE_ROTATION_SUPPORT Jan 01 00:00:00.596 screen.94225 slog 300 screen: loading libhiddi.so... Jan 01 00:00:00.596 screen.94225 slog 300 screen: server is ready J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# pidin ar pid Arguments 1 procnto-smp-instr -v 2 pipe 3 slogger2 4 dumper -d /tmp 5 random -t 6 devc-seromap -e -F 0x02800000,224 7 i2c-omap35xx -p0x2000000 -i232 -d 8 i2c-omap35xx -p0x2010000 -i233 -d 9 devb-sdmmc-am65x blk cache=1m sdio addr=0x4f80000,irq=35,timing=~hs400,emmc,bs=sscfg=0x8000 disk name=emmc 49162 devb-sdmmc-am65x blk noatime,cache=8M,automount=@/proc/boot/automount cam cache,async,quiet,pnp sdio addr=0x04fb0000,irq=36,bs=sscfg=0x8000:ldo=0x600000^117 dos exe=all disk name=sd1 61451 io-usb-otg -d xhci ioport=0x6010000,irq=128,iosize=65536,nousb3 61452 ksh /proc/boot/.console_ti.sh 69645 tisci-mgr 81934 shmemallocator 86031 tiipc-mgr 90128 tiudma-mgr 94225 screen -c /sd/usr/lib/graphics/jacinto7/graphics.conf.dss_on_r5 98322 ksh ksh 155667 pidin ar J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# J7EVM@QNX:/# gle gles1 gles1-v gles1-vsync Read BVNC 22.104.208.318 from HW device registers RGX Device initialised with BVNC 22.104.208.318 J7EVM@QNX:/#

Regards,
Gokul