This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDA4VMXEVM: Utilization of VPAC/DMPAC for generic Image Processing.

Part Number: TDA4VMXEVM

Tool/software: TI C/C++ Compiler

Hi,

On studying through the VPAC (In particular the MSC) TIVX Kernel we could find that it is specifically designed to support an image format i.e NV12, RGB. If we've a different format other than that of the supported list from the pdk/hwa. How to start developing/getting support for this?

For ex: YUYV is the input image format and we'd like to use VPAC_MSC to scale the input image down a size. We've the kernel developed, of course it did'nt work on going through more details of this. The way to develope a VPAC kernel is different since it works closely with the FVID2 layer and controlled by the configuration params.

The question here would be.

1. Can we support a different format other than the ones available within the SDK to use the VPAC/DMPAC h/w accelerators?

2. If so, how? If not, any other alternative other than changing the camera formats

Sriram,

Visteon Corporation