Other Parts Discussed in Thread: OMAPL138
Tool/software: Code Composer Studio
Hello,
We are planning on using the C6654 as a medium-voltage system controller. The team has plenty of experience with the C2000 series but close to none with the C6000 series. We do plan on the C6654 DSP to run calculations (calculate duty cycle, phase shift, etc.) and transmit the data to an FPGA using the uPP interface.
I have been searching for a base project (similar to C2000 examples) that contains just the necessities, such as PLL, to run the desired peripheral.
I did download the SDK (ti-processor-sdk-rtos-c665x-evm-06.03.00.106-Windows-x86-Install) but I am not interesting in RTOS - the code will need to run with sub-us precision timing and such bare-metal is our choice.
Thank you,
Tomas