This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDA2HV: NDK project fall after reload project

Part Number: TDA2HV


Tool/software: Code Composer Studio

We work with NDK and NSP. Project create in CCS 9.x. When the project is first launched - everything is OK. When reload program occurs the next exception:

[CortexA15_0] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x80a2f770.
Main stack size: 0x1000.
R0 = 0x00000001  R8  = 0x4037ffbc
R1 = 0x600001df  R9  = 0xffffffff
R2 = 0x00000001  R10 = 0x00000000
R3 = 0x4ae0c204  R11 = 0x80a3073c
R4 = 0x00000001  R12 = 0x800001df
R5 = 0x8095ba44  SP(R13) = 0x80920418
R6 = 0x00000001  LR(R14) = 0x80a2dd84
R7 = 0x80a30770  PC(R15) = 0x80920418
PSR = 0xffffffff
DFSR = 0x00000206  IFSR = 0x00000000
DFAR = 0x4ae0c204  IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x80920418, lr = 0x80a2dd84.
xdc.runtime.Error.raise: terminating execution

What could be the reason for this fall? If we make power recycle - everything OK and project run as first time.

SYSBIOS: 6.46.06.00
CCS: 9.3
NDK: 2.24.02.31
NSP: nsp gmacsw 4_16_01_01
SDK: VISION SDK 3.08
XDS: xdctools 3.32.01.22
Device: TDA2HV