This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DRA829]Ospi startup mode clock frequency setting

Other Parts Discussed in Thread: DRA829

Hi, Experts,

1.I saw in the 4.3.4 OSPI Boot Device Configuration section of the manual that configuring the BOOTMODE-6 pin can set the speed in OSPI mode, 0 = 33MHz; 1 = 133MHz;

2.When I set BOOTMODE-6 pin = 0, does 33MHz refer to the output clock of OSPI?

So when I set BOOTMODE-6 pin = 1, does 133MHz mean the output clock of OSPI? Or is this 133MHz the reference clock internally further divided into other frequencies?
Regards,

Xie