Part Number: TDA4VM
Questions from customer regarding TDA4VM SERDES_RX/TX pins.
1. Can SERDES_RX/TX can be float if they are not used?
2. If SERDES is not used, will SERDES REFCLK source be needed?
3. For example, PCIE and SGMII pins can be float if they are not used, correct?
4. Do they still need to provide clk source to REFCLK?
5. Is pull down resistor of SERDES_REXT needed? Please see figure below