This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Logic PD Zoom OMAP35x Development Kit_Booting Issue

Hello,

Can any one help on below issue?

We use Logic PD Zoom OMAP35x Development Kit. The OMAP processor is not loading Win CE image on power up. It loads the LoLo and runs idle thread. It is able to load the Win CE image if load command is issued through LoLo. By default the boot priority is for SD card. We tried writing a script in to config block to load the Win CE image from SD card. Since the config block is available only for NAND it works if the boot priority is altered either by changing the boot strap resistor settings or by inserting the SD card after the NAND boot is initiated. We want to confirm exactly where the issue is rather than bypassing it by above method, is it hardware related or the SD card is corrupted?


Regards,

Thomas