Hello,
We are designing a custom carrier board for Logic PDs OMAP35x SOM-LV. Due to some design constraints we are forced to use some of the GPIOs which are not recommended by Logic PD to use as GPIOs. Below are the details of signals we use as GPIOs. Violated signals are highlighted in red and partially used modules are highlighted in violet. Whether we can use them based on the criteria mentioned in 'Function In Design' and 'Module Usage In Design' columns?
Please check the attachment if the table is not proper
Regards,
Thomas
Sl No | SOM Signal Name | SOM Connector Pin Number | OMAP Ball | Planned Use |
Function In Design | Direction WRT SOM | OMAP Module | Module Usage In Design |
1 | uP_UARTC_CTS | J1-122 | AB26 | GPIO_144 | Peripheral interrupt input | IN | UARTC | UARTC is not used in design, The interfaces to WiFi and BT chips are not implemented in SOM (R121 and R18 not populated) |
2 | uP_UARTC_RTS | J1-124 | AB25 | GPIO_145 | Peripheral enable signal | OUT | UARTC | UARTC is not used in design, The interfaces to WiFi and BT chips are not implemented in SOM (R121 and R18 not populated) |
3 | uP_UARTC_RX | J1-126 | AD25 | GPIO_147 | Peripheral interrupt input | IN | UARTC | UARTC is not used in design, The interfaces to WiFi and BT chips are not implemented in SOM (R121 and R18 not populated) |
4 | uP_UARTB_CTS | J1-136 | H18 | GPIO_163 | Peripheral interrupt input | IN | UARTB | UARTB is used in null modem configuration |
5 | uP_UARTB_RTS | J1-138 | H19 | GPIO_164 | Peripheral enable signal | OUT | UARTB | UARTB is used in null modem configuration |
6 | uP_GPIO3 | J1-142 | B26 | GPIO_111 | Peripheral enable signal | OUT | GPIO | GPIO |
7 | uP_GPIO2 | J1-166 | AA10 | GPIO_31 | Peripheral enable signal | OUT | GPIO | GPIO |
8 | uP_SPI_CS1 | J1-220 | AF4 | GPIO_135 | Peripheral interrupt input | IN | SPI | SPI is not used in design |
9 | uP_SPI_CS0 | J1-222 | AG4 | GPIO_134 | Peripheral interrupt input | IN | SPI | SPI is not used in design |
10 | uP_SPI_SOMI | J1-224 | AH5 | GPIO_132 | Peripheral interrupt input | IN | SPI | SPI is not used in design |
11 | uP_SPI_SIMO | J1-226 | AG5 | GPIO_131 | Peripheral interrupt input | IN | SPI | SPI is not used in design |
12 | uP_SPI_SCLK | J1-228 | AE2 | GPIO_130 | Peripheral enable signal | OUT | SPI | SPI is not used in design, 22E termination in SOM is ignorable |