Hello,
i would know if Multicast option exists in DiretIO for RapidIO v1.2 ?
thank you in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
i would know if Multicast option exists in DiretIO for RapidIO v1.2 ?
thank you in advance.
The original SRIO v1.2 spec. only specified multicast-event capability, which is differenet from packet multicast capability. I assume that you asked for the packet multicast capability. The packet multicast feature was not part of the original SRIO 1.2v spec. release. And it was presented as a seperate spec. from the main SRIO1.2v. It became part of main SRIO spec. at version 1.3. So the multicast option does exist in RapidIP v1.2.
Since the multicast capability is an extended feature for SRIO, the vendor can choose not to implement. You can find out whether the device supports multicast capability or not through the bit 21 of Processing elements feature CAR register ( config space offset at 0x10).
I hope it is helpful.
Regards,
Chunhua
Yes, NWRITE and SWRITE transactions can be used with Multicast.
Regards,
Travis