Hi, We are part of Burlington design team and working on the OMAP4430 and we have the follwing questions
How we can adjust (modify) the amplitude of USB output (USBAB0_OTG_DM, USBAB0_OTG_DP) thru USB driver or writing directly into the registers.
How we can configure the USB to operate as USB1.0 having a clock rate 12 MHz (at DM and DP). We do not want to have any USB 2.0 and backward rate operational
Zia Zabihi
Sr. System Architect
FLEXTRONICS Canada Design Services
+1 613.895.2050 x2692
zia.zabihi@ca.flextronics.com