Hi,
What is the maximum trace length that can used to route VOUT traces from the possessor to an LCD connector without using a buffer device?
-Thariq
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the maximum trace length that can used to route VOUT traces from the possessor to an LCD connector without using a buffer device?
-Thariq
Hi Thariq,
We do not have a maximum trace length spec. In the datasheet, the LVCMOS drivers have an output impedance of 40 ohm, and drive strength of 6ma minimum. It would be advisable to run simulations on your design to ensure you have enough margin.
Regards,
Mike