We would like to reduce unit power draw to <2.5mA during USB suspend with a DM365 powered from the USB bus 5V supply. Does anybody know if it is possible to do this with any of the supplied power down/sleep modes provided by the DM365? We would like to keep D+ pulled up while in USB suspend to stay attached so that the unit will wake up when the computer is brought out of standby/sleep/suspend, and to my knowledge, the maximum current draw is 2.5mA on the USB Vbus while in suspend mode.
Thanks,
Andrew