This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: UBoot Environment File is not working

Part Number: TDA4VM


Hi,

I am flashing u-boot.img and u-boot-env file to SPI Flash memory using below instructions:

Uboot> setenv dfu_alt_info ${dfu_alt_info_ospi}

Uboot> sf probe 0

#SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB

Uboot> dfu 0 sf 0:0:64000000:0

host#sudo dfu-util -c 1 -i 0 -a 3 -D u-boot-env (along with other bootloaders).

The u-boot.img was configured as 'SPI Flash' for saving environment in the menuconfig. And the bootcmd was changed to load kernel from eMMC memory.

Similarly, the u-boot.-env (generated using mkevnImage tool) was also having bootcmd as to load from eMMC memory.

But, when we boot the board after flashing these things.  But, if we print the bootcmd value in Uboot prompt. It is printing something else which is to load from sd card. The uboot log says that it loaded environment from SPI Flash.

I am not able to find, from which location the Uboot is fetching these bootcmd values, which I have not given either in uboot.img or u-boot-env file.

Kindly provide some help.

Thank you.

Regards,

Sainath

  • Hi Sainath,

    Any particular reason for why you are not shifting entirely to eMMC? 

    U-boot + Linux + filesystem on eMMC?

    If in case you want u-boot in OSPI & Linux+FS on eMMC can you share the u-boot config
    that you are using? I will try to reproduce that locally in my setup.

    Best Regards,
    Keerthy

  • Hi,

    Our requirement says that Uboot should be in OSPI and Linux+RootFS on eMMC.

    So, as per this, we want to flash default u-boot environment to OSPI and expect Uboot to use this environment.

    Please find the Uboot .config file. Also attached my u-boot-env file which is being flashing to OSPI and also its corresponding uboot env text file.

    PS) Attached files: .config -> mydotconfig.txt , ubootenv.txt, u-boot-env -> u-boot-env.txt

    Thank you.

    Best Regards,

    Sainath

    #
    # Automatically generated file; DO NOT EDIT.
    # U-Boot 2019.01 Configuration
    #
    CONFIG_CREATE_ARCH_SYMLINK=y
    # CONFIG_ARC is not set
    CONFIG_ARM=y
    # CONFIG_M68K is not set
    # CONFIG_MICROBLAZE is not set
    # CONFIG_MIPS is not set
    # CONFIG_NDS32 is not set
    # CONFIG_NIOS2 is not set
    # CONFIG_PPC is not set
    # CONFIG_RISCV is not set
    # CONFIG_SANDBOX is not set
    # CONFIG_SH is not set
    # CONFIG_X86 is not set
    # CONFIG_XTENSA is not set
    CONFIG_SYS_ARCH="arm"
    CONFIG_SYS_CPU="armv8"
    CONFIG_SYS_SOC="k3"
    CONFIG_SYS_VENDOR="ti"
    CONFIG_SYS_BOARD="j721e"
    CONFIG_SYS_CONFIG_NAME="j721e_evm"
    CONFIG_SYS_DISABLE_DCACHE_OPS=y
    
    #
    # ARM architecture
    #
    CONFIG_ARM64=y
    # CONFIG_POSITION_INDEPENDENT is not set
    CONFIG_STATIC_RELA=y
    CONFIG_DMA_ADDR_T_64BIT=y
    CONFIG_ARM_ASM_UNIFIED=y
    # CONFIG_SYS_ARM_CACHE_CP15 is not set
    # CONFIG_SYS_ARM_MMU is not set
    # CONFIG_SYS_ARM_MPU is not set
    CONFIG_SYS_ARM_ARCH=8
    CONFIG_SYS_CACHE_SHIFT_6=y
    CONFIG_SYS_CACHELINE_SIZE=64
    CONFIG_SYS_ARCH_TIMER=y
    CONFIG_ARM_SMCCC=y
    # CONFIG_SEMIHOSTING is not set
    # CONFIG_SYS_L2CACHE_OFF is not set
    # CONFIG_ENABLE_ARM_SOC_BOOT0_HOOK is not set
    CONFIG_ARM64_SUPPORT_AARCH32=y
    # CONFIG_ARCH_AT91 is not set
    # CONFIG_TARGET_EDB93XX is not set
    # CONFIG_TARGET_ASPENITE is not set
    # CONFIG_TARGET_GPLUGD is not set
    # CONFIG_ARCH_DAVINCI is not set
    # CONFIG_KIRKWOOD is not set
    # CONFIG_ARCH_MVEBU is not set
    # CONFIG_TARGET_APF27 is not set
    # CONFIG_ORION5X is not set
    # CONFIG_TARGET_SPEAR300 is not set
    # CONFIG_TARGET_SPEAR310 is not set
    # CONFIG_TARGET_SPEAR320 is not set
    # CONFIG_TARGET_SPEAR600 is not set
    # CONFIG_TARGET_STV0991 is not set
    # CONFIG_TARGET_X600 is not set
    # CONFIG_TARGET_WOODBURN is not set
    # CONFIG_TARGET_WOODBURN_SD is not set
    # CONFIG_TARGET_FLEA3 is not set
    # CONFIG_TARGET_MX35PDK is not set
    # CONFIG_ARCH_BCM283X is not set
    # CONFIG_ARCH_BCM6858 is not set
    # CONFIG_TARGET_VEXPRESS_CA15_TC2 is not set
    # CONFIG_ARCH_BCMSTB is not set
    # CONFIG_TARGET_VEXPRESS_CA5X2 is not set
    # CONFIG_TARGET_VEXPRESS_CA9X4 is not set
    # CONFIG_TARGET_BCM23550_W1D is not set
    # CONFIG_TARGET_BCM28155_AP is not set
    # CONFIG_TARGET_BCMCYGNUS is not set
    # CONFIG_TARGET_BCMNSP is not set
    # CONFIG_TARGET_BCMNS2 is not set
    # CONFIG_ARCH_EXYNOS is not set
    # CONFIG_ARCH_S5PC1XX is not set
    # CONFIG_ARCH_HIGHBANK is not set
    # CONFIG_ARCH_INTEGRATOR is not set
    # CONFIG_ARCH_KEYSTONE is not set
    CONFIG_ARCH_K3=y
    # CONFIG_ARCH_OMAP2PLUS is not set
    # CONFIG_ARCH_MESON is not set
    # CONFIG_ARCH_MEDIATEK is not set
    # CONFIG_ARCH_LPC32XX is not set
    # CONFIG_ARCH_IMX8 is not set
    # CONFIG_ARCH_IMX8M is not set
    # CONFIG_ARCH_MX23 is not set
    # CONFIG_ARCH_MX25 is not set
    # CONFIG_ARCH_MX28 is not set
    # CONFIG_ARCH_MX31 is not set
    # CONFIG_ARCH_MX7ULP is not set
    # CONFIG_ARCH_MX7 is not set
    # CONFIG_ARCH_MX6 is not set
    CONFIG_SPL_LDSCRIPT="arch/arm/cpu/armv8/u-boot-spl.lds"
    # CONFIG_ARCH_MX5 is not set
    # CONFIG_ARCH_OWL is not set
    # CONFIG_ARCH_QEMU is not set
    # CONFIG_ARCH_RMOBILE is not set
    # CONFIG_TARGET_S32V234EVB is not set
    # CONFIG_ARCH_SNAPDRAGON is not set
    # CONFIG_ARCH_SOCFPGA is not set
    # CONFIG_ARCH_SUNXI is not set
    # CONFIG_ARCH_VERSAL is not set
    # CONFIG_ARCH_VF610 is not set
    # CONFIG_ARCH_ZYNQ is not set
    # CONFIG_ARCH_ZYNQMP_R5 is not set
    # CONFIG_ARCH_ZYNQMP is not set
    # CONFIG_TEGRA is not set
    # CONFIG_TARGET_VEXPRESS64_AEMV8A is not set
    # CONFIG_TARGET_VEXPRESS64_BASE_FVP is not set
    # CONFIG_TARGET_VEXPRESS64_BASE_FVP_DRAM is not set
    # CONFIG_TARGET_VEXPRESS64_JUNO is not set
    # CONFIG_TARGET_LS2080A_EMU is not set
    # CONFIG_TARGET_LS2080A_SIMU is not set
    # CONFIG_TARGET_LS1088AQDS is not set
    # CONFIG_TARGET_LS2080AQDS is not set
    # CONFIG_TARGET_LS2080ARDB is not set
    # CONFIG_TARGET_LS2081ARDB is not set
    # CONFIG_TARGET_HIKEY is not set
    # CONFIG_TARGET_POPLAR is not set
    # CONFIG_TARGET_LS1012AQDS is not set
    # CONFIG_TARGET_LS1012ARDB is not set
    # CONFIG_TARGET_LS1012A2G5RDB is not set
    # CONFIG_TARGET_LS1012AFRWY is not set
    # CONFIG_TARGET_LS1012AFRDM is not set
    # CONFIG_TARGET_LS1088ARDB is not set
    # CONFIG_TARGET_LS1021AQDS is not set
    # CONFIG_TARGET_LS1021ATWR is not set
    # CONFIG_TARGET_LS1021AIOT is not set
    # CONFIG_TARGET_LS1043AQDS is not set
    # CONFIG_TARGET_LS1043ARDB is not set
    # CONFIG_TARGET_LS1046AQDS is not set
    # CONFIG_TARGET_LS1046ARDB is not set
    # CONFIG_TARGET_H2200 is not set
    # CONFIG_TARGET_ZIPITZ2 is not set
    # CONFIG_TARGET_COLIBRI_PXA270 is not set
    # CONFIG_ARCH_UNIPHIER is not set
    # CONFIG_STM32 is not set
    # CONFIG_ARCH_STI is not set
    # CONFIG_ARCH_STM32MP is not set
    # CONFIG_ARCH_ROCKCHIP is not set
    # CONFIG_TARGET_THUNDERX_88XX is not set
    # CONFIG_ARCH_ASPEED is not set
    # CONFIG_TI_SECURE_DEVICE is not set
    CONFIG_SYS_TEXT_BASE=0x80800000
    CONFIG_TI_I2C_BOARD_DETECT=y
    CONFIG_EEPROM_BUS_ADDRESS=0
    CONFIG_EEPROM_CHIP_ADDRESS=0x50
    # CONFIG_TI_COMMON_CMD_OPTIONS is not set
    CONFIG_SPL_GPIO_SUPPORT=y
    CONFIG_SPL_LIBCOMMON_SUPPORT=y
    CONFIG_SPL_LIBGENERIC_SUPPORT=y
    CONFIG_SYS_MALLOC_F_LEN=0x8000
    # CONFIG_SOC_K3_AM6 is not set
    CONFIG_SOC_K3_J721E=y
    CONFIG_SYS_K3_NON_SECURE_MSRAM_SIZE=0x100000
    CONFIG_SYS_K3_MAX_DOWNLODABLE_IMAGE_SIZE=0xc0000
    CONFIG_SYS_K3_MCU_SCRATCHPAD_BASE=0x40280000
    CONFIG_SYS_K3_MCU_SCRATCHPAD_SIZE=0x200
    CONFIG_SYS_K3_BOOT_PARAM_TABLE_INDEX=0x41cffbfc
    CONFIG_SYS_K3_KEY=""
    CONFIG_SYS_K3_BOOT_CORE_ID=16
    # CONFIG_K3_EARLY_CONS is not set
    CONFIG_TARGET_J721E_A72_EVM=y
    # CONFIG_TARGET_J721E_R5_EVM is not set
    # CONFIG_TFABOOT is not set
    CONFIG_SPL_MMC_SUPPORT=y
    CONFIG_SPL_SERIAL_SUPPORT=y
    CONFIG_SPL_DRIVERS_MISC_SUPPORT=y
    CONFIG_SPL_SYS_MALLOC_F_LEN=0x8000
    CONFIG_SPL=y
    CONFIG_IDENT_STRING=""
    CONFIG_SPL_STACK_R_ADDR=0x82000000
    CONFIG_SPL_FAT_SUPPORT=y
    CONFIG_SPL_LIBDISK_SUPPORT=y
    CONFIG_SPL_SPI_FLASH_SUPPORT=y
    CONFIG_SPL_SPI_SUPPORT=y
    CONFIG_ARMV8_SPL_EXCEPTION_VECTORS=y
    # CONFIG_ARMV8_MULTIENTRY is not set
    # CONFIG_ARMV8_SET_SMPEN is not set
    
    #
    # ARMv8 secure monitor firmware
    #
    # CONFIG_ARMV8_SEC_FIRMWARE_SUPPORT is not set
    # CONFIG_SPL_ARMV8_SEC_FIRMWARE_SUPPORT is not set
    CONFIG_PSCI_RESET=y
    # CONFIG_ARMV8_PSCI is not set
    # CONFIG_ARMV8_EA_EL3_FIRST is not set
    # CONFIG_CMD_DEKBLOB is not set
    # CONFIG_CMD_HDMIDETECT is not set
    
    #
    # ARM debug
    #
    CONFIG_SMBIOS_PRODUCT_NAME="j721e"
    # CONFIG_DEBUG_UART is not set
    # CONFIG_AHCI is not set
    
    #
    # General setup
    #
    CONFIG_LOCALVERSION=""
    CONFIG_LOCALVERSION_AUTO=y
    CONFIG_CC_OPTIMIZE_FOR_SIZE=y
    CONFIG_DISTRO_DEFAULTS=y
    CONFIG_ENV_VARS_UBOOT_CONFIG=y
    CONFIG_NR_DRAM_BANKS=2
    # CONFIG_SYS_BOOT_GET_CMDLINE is not set
    # CONFIG_SYS_BOOT_GET_KBD is not set
    CONFIG_SYS_MALLOC_F=y
    CONFIG_TPL_SYS_MALLOC_F_LEN=0x8000
    CONFIG_EXPERT=y
    # CONFIG_SYS_MALLOC_CLEAR_ON_INIT is not set
    # CONFIG_TOOLS_DEBUG is not set
    CONFIG_PHYS_64BIT=y
    
    #
    # Boot images
    #
    CONFIG_ANDROID_BOOT_IMAGE=y
    CONFIG_FIT=y
    CONFIG_FIT_EXTERNAL_OFFSET=0x0
    CONFIG_FIT_ENABLE_SHA256_SUPPORT=y
    # CONFIG_FIT_SIGNATURE is not set
    # CONFIG_FIT_VERBOSE is not set
    # CONFIG_FIT_BEST_MATCH is not set
    CONFIG_SPL_FIT=y
    # CONFIG_SPL_FIT_PRINT is not set
    # CONFIG_SPL_FIT_SIGNATURE is not set
    CONFIG_SPL_LOAD_FIT=y
    # CONFIG_SPL_LOAD_FIT_FULL is not set
    # CONFIG_SPL_FIT_IMAGE_POST_PROCESS is not set
    CONFIG_SPL_FIT_SOURCE=""
    CONFIG_SPL_FIT_GENERATOR=""
    CONFIG_IMAGE_FORMAT_LEGACY=y
    CONFIG_OF_BOARD_SETUP=y
    # CONFIG_OF_SYSTEM_SETUP is not set
    # CONFIG_OF_STDOUT_VIA_ALIAS is not set
    CONFIG_SYS_EXTRA_OPTIONS=""
    CONFIG_ARCH_FIXUP_FDT_MEMORY=y
    
    #
    # API
    #
    # CONFIG_API is not set
    
    #
    # Boot timing
    #
    # CONFIG_BOOTSTAGE is not set
    CONFIG_BOOTSTAGE_RECORD_COUNT=30
    CONFIG_SPL_BOOTSTAGE_RECORD_COUNT=5
    CONFIG_BOOTSTAGE_STASH_ADDR=0
    CONFIG_BOOTSTAGE_STASH_SIZE=0x1000
    
    #
    # Boot media
    #
    # CONFIG_NAND_BOOT is not set
    # CONFIG_ONENAND_BOOT is not set
    # CONFIG_QSPI_BOOT is not set
    # CONFIG_SATA_BOOT is not set
    # CONFIG_SD_BOOT is not set
    CONFIG_SPI_BOOT=y
    CONFIG_BOOTDELAY=2
    CONFIG_USE_BOOTARGS=y
    CONFIG_BOOTARGS="console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 vm.overcommit_ratio=5 vm.overcommit_memory=2 root=/dev/mmcblk0p1 ip=dhcp"
    CONFIG_USE_BOOTCOMMAND=y
    CONFIG_BOOTCOMMAND="setenv autoload no;ext4load mmc 0:1 0x82000000 /boot/Image;ext4load mmc 0:1 0x81200000 /boot/k3-j721e-common-proc-board.dtb; booti 0x82000000 - 0x81200000"
    
    #
    # Console
    #
    CONFIG_MENU=y
    # CONFIG_CONSOLE_RECORD is not set
    # CONFIG_DISABLE_CONSOLE is not set
    CONFIG_LOGLEVEL=4
    CONFIG_SPL_LOGLEVEL=4
    CONFIG_TPL_LOGLEVEL=4
    # CONFIG_SILENT_CONSOLE is not set
    # CONFIG_PRE_CONSOLE_BUFFER is not set
    # CONFIG_CONSOLE_MUX is not set
    # CONFIG_SYS_CONSOLE_IS_IN_ENV is not set
    # CONFIG_SYS_CONSOLE_OVERWRITE_ROUTINE is not set
    # CONFIG_SYS_CONSOLE_ENV_OVERWRITE is not set
    # CONFIG_SYS_CONSOLE_INFO_QUIET is not set
    # CONFIG_SYS_STDIO_DEREGISTER is not set
    
    #
    # Logging
    #
    # CONFIG_LOG is not set
    CONFIG_SUPPORT_RAW_INITRD=y
    CONFIG_DEFAULT_FDT_FILE=""
    # CONFIG_MISC_INIT_R is not set
    # CONFIG_VERSION_VARIABLE is not set
    CONFIG_BOARD_LATE_INIT=y
    CONFIG_DISPLAY_CPUINFO=y
    CONFIG_DISPLAY_BOARDINFO=y
    # CONFIG_DISPLAY_BOARDINFO_LATE is not set
    
    #
    # Start-up hooks
    #
    # CONFIG_ARCH_EARLY_INIT_R is not set
    # CONFIG_ARCH_MISC_INIT is not set
    # CONFIG_BOARD_EARLY_INIT_F is not set
    # CONFIG_BOARD_EARLY_INIT_R is not set
    # CONFIG_LAST_STAGE_INIT is not set
    
    #
    # Security support
    #
    CONFIG_HASH=y
    
    #
    # Update support
    #
    # CONFIG_UPDATE_TFTP is not set
    
    #
    # Blob list
    #
    # CONFIG_BLOBLIST is not set
    
    #
    # SPL / TPL
    #
    CONFIG_SUPPORT_SPL=y
    CONFIG_SPL_DFU_NO_RESET=y
    CONFIG_SPL_FRAMEWORK=y
    CONFIG_SPL_BOARD_INIT=y
    # CONFIG_SPL_BOOTROM_SUPPORT is not set
    # CONFIG_SPL_BOOTCOUNT_LIMIT is not set
    CONFIG_SPL_RAW_IMAGE_SUPPORT=y
    CONFIG_SPL_LEGACY_IMAGE_SUPPORT=y
    CONFIG_SPL_SYS_MALLOC_SIMPLE=y
    # CONFIG_TPL_SYS_MALLOC_SIMPLE is not set
    CONFIG_SPL_STACK_R=y
    CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN=0x100000
    CONFIG_SPL_SEPARATE_BSS=y
    CONFIG_SPL_BANNER_PRINT=y
    CONFIG_TPL_BANNER_PRINT=y
    # CONFIG_SPL_DISPLAY_PRINT is not set
    CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR=y
    CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_SECTOR=0x1400
    # CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_PARTITION is not set
    # CONFIG_SPL_CRC32_SUPPORT is not set
    # CONFIG_SPL_MD5_SUPPORT is not set
    # CONFIG_SPL_SHA1_SUPPORT is not set
    # CONFIG_SPL_SHA256_SUPPORT is not set
    # CONFIG_SPL_FIT_IMAGE_TINY is not set
    # CONFIG_SPL_CPU_SUPPORT is not set
    # CONFIG_SPL_CRYPTO_SUPPORT is not set
    CONFIG_SPL_HASH_SUPPORT=y
    # CONFIG_TPL_HASH_SUPPORT is not set
    CONFIG_SPL_DMA=y
    CONFIG_SPL_ENV_SUPPORT=y
    # CONFIG_SPL_SAVEENV is not set
    # CONFIG_SPL_ETH_SUPPORT is not set
    # CONFIG_SPL_EXT_SUPPORT is not set
    # CONFIG_SPL_FPGA_SUPPORT is not set
    CONFIG_SPL_I2C_SUPPORT=y
    CONFIG_SPL_DM_MAILBOX=y
    # CONFIG_SPL_MMC_WRITE is not set
    # CONFIG_SPL_MPC8XXX_INIT_DDR_SUPPORT is not set
    CONFIG_SPL_MTD_SUPPORT=y
    # CONFIG_SPL_MUSB_NEW_SUPPORT is not set
    # CONFIG_SPL_NAND_SUPPORT is not set
    # CONFIG_SPL_NET_SUPPORT is not set
    # CONFIG_SPL_NO_CPU_SUPPORT is not set
    CONFIG_SPL_NOR_SUPPORT=y
    # CONFIG_SPL_XIP_SUPPORT is not set
    # CONFIG_SPL_ONENAND_SUPPORT is not set
    # CONFIG_SPL_OS_BOOT is not set
    CONFIG_SPL_PAYLOAD="u-boot.bin"
    # CONFIG_SPL_PCI is not set
    # CONFIG_SPL_PCH_SUPPORT is not set
    # CONFIG_SPL_POST_MEM_SUPPORT is not set
    CONFIG_SPL_DM_RESET=y
    CONFIG_SPL_POWER_SUPPORT=y
    CONFIG_SPL_POWER_DOMAIN=y
    CONFIG_SPL_RAM_SUPPORT=y
    CONFIG_SPL_RAM_DEVICE=y
    # CONFIG_SPL_REMOTEPROC is not set
    # CONFIG_SPL_RTC_SUPPORT is not set
    # CONFIG_SPL_SATA_SUPPORT is not set
    # CONFIG_SPL_SPI_FLASH_TINY is not set
    CONFIG_SPL_SPI_FLASH_SFDP_SUPPORT=y
    CONFIG_SPL_SPI_LOAD=y
    # CONFIG_SPL_THERMAL is not set
    # CONFIG_SPL_USB_HOST_SUPPORT is not set
    CONFIG_SPL_USB_GADGET=y
    # CONFIG_SPL_USB_ETHER is not set
    CONFIG_SPL_DFU=y
    CONFIG_SPL_DFU_RAM=y
    # CONFIG_SPL_USB_SDP_SUPPORT is not set
    # CONFIG_SPL_WATCHDOG_SUPPORT is not set
    CONFIG_SPL_YMODEM_SUPPORT=y
    # CONFIG_SPL_ATF is not set
    # CONFIG_SPL_AM33XX_ENABLE_RTC32K_OSC is not set
    # CONFIG_SPL_OPTEE is not set
    
    #
    # Command line interface
    #
    CONFIG_CMDLINE=y
    CONFIG_HUSH_PARSER=y
    CONFIG_CMDLINE_EDITING=y
    CONFIG_AUTO_COMPLETE=y
    CONFIG_SYS_LONGHELP=y
    CONFIG_SYS_PROMPT="=> "
    
    #
    # Autoboot options
    #
    CONFIG_AUTOBOOT=y
    # CONFIG_AUTOBOOT_KEYED is not set
    
    #
    # Commands
    #
    
    #
    # Info commands
    #
    CONFIG_CMD_BDI=y
    # CONFIG_CMD_CONFIG is not set
    CONFIG_CMD_CONSOLE=y
    # CONFIG_CMD_CPU is not set
    # CONFIG_CMD_LICENSE is not set
    
    #
    # Boot commands
    #
    CONFIG_CMD_BOOTD=y
    CONFIG_CMD_BOOTM=y
    # CONFIG_CMD_BOOTZ is not set
    CONFIG_CMD_BOOTI=y
    CONFIG_CMD_BOOTEFI=y
    CONFIG_CMD_BOOTEFI_HELLO_COMPILE=y
    # CONFIG_CMD_BOOTEFI_HELLO is not set
    # CONFIG_CMD_BOOTEFI_SELFTEST is not set
    # CONFIG_CMD_BOOTMENU is not set
    # CONFIG_CMD_DTIMG is not set
    CONFIG_CMD_ELF=y
    CONFIG_CMD_FDT=y
    CONFIG_CMD_GO=y
    CONFIG_CMD_RUN=y
    CONFIG_CMD_IMI=y
    # CONFIG_CMD_IMLS is not set
    CONFIG_CMD_XIMG=y
    # CONFIG_CMD_SPL is not set
    # CONFIG_CMD_FITUPD is not set
    # CONFIG_CMD_THOR_DOWNLOAD is not set
    # CONFIG_CMD_ZBOOT is not set
    
    #
    # Environment commands
    #
    CONFIG_CMD_ASKENV=y
    CONFIG_CMD_EXPORTENV=y
    CONFIG_CMD_IMPORTENV=y
    CONFIG_CMD_EDITENV=y
    # CONFIG_CMD_GREPENV is not set
    CONFIG_CMD_SAVEENV=y
    CONFIG_CMD_ENV_EXISTS=y
    # CONFIG_CMD_ENV_CALLBACK is not set
    # CONFIG_CMD_ENV_FLAGS is not set
    
    #
    # Memory commands
    #
    # CONFIG_CMD_BINOP is not set
    CONFIG_CMD_CRC32=y
    # CONFIG_CRC32_VERIFY is not set
    # CONFIG_LOOPW is not set
    # CONFIG_CMD_MD5SUM is not set
    # CONFIG_CMD_MEMINFO is not set
    CONFIG_CMD_MEMORY=y
    # CONFIG_CMD_MEMTEST is not set
    # CONFIG_CMD_MX_CYCLIC is not set
    # CONFIG_CMD_SHA1SUM is not set
    # CONFIG_CMD_STRINGS is not set
    
    #
    # Compression commands
    #
    CONFIG_CMD_LZMADEC=y
    CONFIG_CMD_UNZIP=y
    # CONFIG_CMD_ZIP is not set
    
    #
    # Device access commands
    #
    # CONFIG_CMD_ARMFLASH is not set
    # CONFIG_CMD_ADC is not set
    # CONFIG_CMD_BIND is not set
    # CONFIG_CMD_CLK is not set
    # CONFIG_CMD_DEMO is not set
    CONFIG_CMD_DFU=y
    # CONFIG_CMD_DM is not set
    CONFIG_CMD_FASTBOOT=y
    # CONFIG_CMD_FDC is not set
    CONFIG_CMD_FLASH=y
    # CONFIG_CMD_FPGAD is not set
    # CONFIG_CMD_FUSE is not set
    CONFIG_CMD_GPIO=y
    CONFIG_CMD_GPT=y
    CONFIG_RANDOM_UUID=y
    # CONFIG_CMD_GPT_RENAME is not set
    # CONFIG_CMD_IDE is not set
    # CONFIG_CMD_IO is not set
    # CONFIG_CMD_IOTRACE is not set
    CONFIG_CMD_I2C=y
    CONFIG_CMD_LOADB=y
    CONFIG_CMD_LOADS=y
    CONFIG_CMD_MMC=y
    # CONFIG_CMD_MMC_RPMB is not set
    # CONFIG_CMD_MMC_SWRITE is not set
    CONFIG_CMD_MTD=y
    # CONFIG_CMD_NAND is not set
    # CONFIG_CMD_MMC_SPI is not set
    # CONFIG_CMD_ONENAND is not set
    # CONFIG_CMD_OSD is not set
    CONFIG_CMD_PART=y
    # CONFIG_CMD_PCI is not set
    # CONFIG_CMD_PCMCIA is not set
    CONFIG_CMD_PINMUX=y
    # CONFIG_CMD_POWEROFF is not set
    # CONFIG_CMD_READ is not set
    CONFIG_CMD_REMOTEPROC=y
    # CONFIG_CMD_SATA is not set
    # CONFIG_CMD_SAVES is not set
    CONFIG_CMD_SCSI=y
    # CONFIG_CMD_SDRAM is not set
    CONFIG_CMD_SF=y
    # CONFIG_CMD_SF_TEST is not set
    # CONFIG_CMD_SPI is not set
    # CONFIG_CMD_TSI148 is not set
    CONFIG_CMD_UFS=y
    # CONFIG_CMD_UNIVERSE is not set
    CONFIG_CMD_USB=y
    # CONFIG_CMD_USB_SDP is not set
    CONFIG_CMD_USB_MASS_STORAGE=y
    
    #
    # Shell scripting commands
    #
    CONFIG_CMD_ECHO=y
    CONFIG_CMD_ITEST=y
    CONFIG_CMD_SOURCE=y
    # CONFIG_CMD_SETEXPR is not set
    CONFIG_CMD_NET=y
    CONFIG_CMD_BOOTP=y
    CONFIG_CMD_DHCP=y
    CONFIG_BOOTP_BOOTPATH=y
    CONFIG_BOOTP_DNS=y
    # CONFIG_BOOTP_DNS2 is not set
    CONFIG_BOOTP_GATEWAY=y
    CONFIG_BOOTP_HOSTNAME=y
    # CONFIG_BOOTP_PREFER_SERVERIP is not set
    CONFIG_BOOTP_SUBNETMASK=y
    # CONFIG_BOOTP_NTPSERVER is not set
    CONFIG_BOOTP_PXE=y
    CONFIG_BOOTP_PXE_CLIENTARCH=0x16
    CONFIG_BOOTP_VCI_STRING="U-Boot.armv8"
    CONFIG_CMD_TFTPBOOT=y
    # CONFIG_CMD_TFTPPUT is not set
    # CONFIG_CMD_TFTPSRV is not set
    CONFIG_NET_TFTP_VARS=y
    # CONFIG_CMD_RARP is not set
    CONFIG_CMD_NFS=y
    CONFIG_CMD_MII=y
    CONFIG_CMD_PING=y
    # CONFIG_CMD_CDP is not set
    # CONFIG_CMD_SNTP is not set
    # CONFIG_CMD_DNS is not set
    # CONFIG_CMD_LINK_LOCAL is not set
    # CONFIG_CMD_ETHSW is not set
    CONFIG_CMD_PXE=y
    # CONFIG_CMD_WOL is not set
    
    #
    # Misc commands
    #
    # CONFIG_CMD_BSP is not set
    # CONFIG_CMD_BKOPS_ENABLE is not set
    CONFIG_CMD_BLOCK_CACHE=y
    # CONFIG_CMD_CACHE is not set
    # CONFIG_CMD_CONITRACE is not set
    # CONFIG_CMD_DISPLAY is not set
    # CONFIG_CMD_LED is not set
    # CONFIG_CMD_DATE is not set
    CONFIG_CMD_TIME=y
    # CONFIG_CMD_GETTIME is not set
    CONFIG_CMD_MISC=y
    # CONFIG_MP is not set
    # CONFIG_CMD_TIMER is not set
    # CONFIG_CMD_QFW is not set
    # CONFIG_CMD_TERMINAL is not set
    # CONFIG_CMD_UUID is not set
    
    #
    # TI specific command line interface
    #
    # CONFIG_CMD_DDR3 is not set
    
    #
    # Power commands
    #
    # CONFIG_CMD_PMIC is not set
    # CONFIG_CMD_REGULATOR is not set
    
    #
    # Security commands
    #
    # CONFIG_CMD_AES is not set
    # CONFIG_CMD_BLOB is not set
    # CONFIG_CMD_HASH is not set
    # CONFIG_CMD_HVC is not set
    # CONFIG_CMD_SMC is not set
    
    #
    # Firmware commands
    #
    
    #
    # Filesystem commands
    #
    # CONFIG_CMD_BTRFS is not set
    CONFIG_CMD_EXT2=y
    CONFIG_CMD_EXT4=y
    CONFIG_CMD_EXT4_WRITE=y
    CONFIG_CMD_FAT=y
    CONFIG_CMD_FS_GENERIC=y
    # CONFIG_CMD_FS_UUID is not set
    # CONFIG_CMD_JFFS2 is not set
    # CONFIG_CMD_MTDPARTS is not set
    CONFIG_MTDIDS_DEFAULT="nor0=47040000.spi.0,nor0=47034000.hyperbus"
    CONFIG_MTDPARTS_DEFAULT="mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs)"
    # CONFIG_CMD_REISER is not set
    # CONFIG_CMD_ZFS is not set
    
    #
    # Debug commands
    #
    # CONFIG_CMD_BEDBUG is not set
    # CONFIG_CMD_DIAG is not set
    # CONFIG_CMD_LOG is not set
    # CONFIG_CMD_TRACE is not set
    CONFIG_CMD_UBI=y
    CONFIG_CMD_UBIFS=y
    
    #
    # Partition Types
    #
    CONFIG_PARTITIONS=y
    # CONFIG_MAC_PARTITION is not set
    # CONFIG_SPL_MAC_PARTITION is not set
    CONFIG_DOS_PARTITION=y
    CONFIG_SPL_DOS_PARTITION=y
    # CONFIG_ISO_PARTITION is not set
    # CONFIG_SPL_ISO_PARTITION is not set
    # CONFIG_AMIGA_PARTITION is not set
    # CONFIG_SPL_AMIGA_PARTITION is not set
    CONFIG_EFI_PARTITION=y
    CONFIG_EFI_PARTITION_ENTRIES_NUMBERS=128
    CONFIG_EFI_PARTITION_ENTRIES_OFF=0
    CONFIG_SPL_EFI_PARTITION=y
    CONFIG_PARTITION_UUIDS=y
    CONFIG_SPL_PARTITION_UUIDS=y
    # CONFIG_PARTITION_TYPE_GUID is not set
    CONFIG_SUPPORT_OF_CONTROL=y
    CONFIG_DTC=y
    
    #
    # Device Tree Control
    #
    CONFIG_OF_CONTROL=y
    # CONFIG_OF_BOARD_FIXUP is not set
    CONFIG_SPL_OF_CONTROL=y
    # CONFIG_OF_LIVE is not set
    CONFIG_OF_SEPARATE=y
    # CONFIG_OF_EMBED is not set
    # CONFIG_OF_BOARD is not set
    # CONFIG_OF_PRIOR_STAGE is not set
    CONFIG_DEFAULT_DEVICE_TREE="k3-j721e-common-proc-board"
    CONFIG_OF_LIST="k3-j721e-common-proc-board k3-j721e-tps65917-proc-board"
    # CONFIG_MULTI_DTB_FIT is not set
    CONFIG_SPL_MULTI_DTB_FIT=y
    CONFIG_SPL_OF_LIST="k3-j721e-common-proc-board k3-j721e-tps65917-proc-board"
    # CONFIG_SPL_MULTI_DTB_FIT_LZO is not set
    # CONFIG_SPL_MULTI_DTB_FIT_GZIP is not set
    CONFIG_SPL_MULTI_DTB_FIT_NO_COMPRESSION=y
    CONFIG_OF_SPL_REMOVE_PROPS="interrupt-parent"
    # CONFIG_SPL_OF_PLATDATA is not set
    CONFIG_MKIMAGE_DTC_PATH="dtc"
    
    #
    # Environment
    #
    # CONFIG_ENV_IS_IN_EEPROM is not set
    # CONFIG_ENV_IS_IN_FAT is not set
    # CONFIG_ENV_IS_IN_EXT4 is not set
    # CONFIG_ENV_IS_IN_FLASH is not set
    # CONFIG_ENV_IS_IN_MMC is not set
    # CONFIG_ENV_IS_IN_NAND is not set
    # CONFIG_ENV_IS_IN_NVRAM is not set
    # CONFIG_ENV_IS_IN_ONENAND is not set
    # CONFIG_ENV_IS_IN_REMOTE is not set
    CONFIG_ENV_IS_IN_SPI_FLASH=y
    # CONFIG_ENV_IS_IN_UBI is not set
    # CONFIG_USE_DEFAULT_ENV_FILE is not set
    # CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG is not set
    # CONFIG_SPL_ENV_IS_NOWHERE is not set
    CONFIG_SPL_ENV_IS_IN_SPI_FLASH=y
    CONFIG_NET=y
    CONFIG_NET_RANDOM_ETHADDR=y
    # CONFIG_NETCONSOLE is not set
    
    #
    # Device Drivers
    #
    
    #
    # Generic Driver Options
    #
    CONFIG_DM=y
    CONFIG_SPL_DM=y
    CONFIG_DM_WARN=y
    # CONFIG_DM_DEBUG is not set
    CONFIG_DM_DEVICE_REMOVE=y
    # CONFIG_SPL_DM_DEVICE_REMOVE is not set
    CONFIG_DM_STDIO=y
    CONFIG_DM_SEQ_ALIAS=y
    CONFIG_SPL_DM_SEQ_ALIAS=y
    CONFIG_REGMAP=y
    CONFIG_SPL_REGMAP=y
    CONFIG_SYSCON=y
    CONFIG_SPL_SYSCON=y
    # CONFIG_DEVRES is not set
    CONFIG_SIMPLE_BUS=y
    CONFIG_SPL_SIMPLE_BUS=y
    CONFIG_OF_TRANSLATE=y
    CONFIG_SPL_OF_TRANSLATE=y
    CONFIG_DM_DEV_READ_INLINE=y
    # CONFIG_ADC is not set
    # CONFIG_ADC_EXYNOS is not set
    # CONFIG_ADC_SANDBOX is not set
    # CONFIG_SARADC_MESON is not set
    # CONFIG_SARADC_ROCKCHIP is not set
    # CONFIG_SATA is not set
    # CONFIG_SCSI_AHCI is not set
    
    #
    # SATA/SCSI device support
    #
    # CONFIG_AHCI_PCI is not set
    # CONFIG_DWC_AHCI is not set
    # CONFIG_DWC_AHSATA is not set
    # CONFIG_FSL_SATA is not set
    # CONFIG_MVSATA_IDE is not set
    # CONFIG_SATA_MV is not set
    # CONFIG_SATA_SIL is not set
    # CONFIG_SATA_SIL3114 is not set
    # CONFIG_AXI is not set
    CONFIG_BLK=y
    CONFIG_HAVE_BLOCK_DEVICE=y
    CONFIG_SPL_BLK=y
    CONFIG_BLOCK_CACHE=y
    # CONFIG_SPL_BLOCK_CACHE is not set
    # CONFIG_IDE is not set
    # CONFIG_BOOTCOUNT_LIMIT is not set
    
    #
    # Clock
    #
    CONFIG_CLK=y
    CONFIG_SPL_CLK=y
    CONFIG_CLK_TI_SCI=y
    # CONFIG_CLK_HSDK is not set
    # CONFIG_CLK_CDCE9XX is not set
    # CONFIG_CLK_AT91 is not set
    # CONFIG_ICS8N3QV01 is not set
    # CONFIG_CLK_MPC83XX is not set
    # CONFIG_CPU is not set
    
    #
    # Hardware crypto devices
    #
    # CONFIG_FSL_CAAM is not set
    # CONFIG_SYS_FSL_SEC_BE is not set
    # CONFIG_SYS_FSL_SEC_LE is not set
    # CONFIG_IMX8M_DRAM is not set
    # CONFIG_IMX8M_LPDDR4 is not set
    # CONFIG_IMX8M_DDR4 is not set
    CONFIG_SAVED_DRAM_TIMING_BASE=0x180000
    
    #
    # Demo for driver model
    #
    # CONFIG_DM_DEMO is not set
    # CONFIG_BOARD is not set
    
    #
    # DFU support
    #
    CONFIG_DFU=y
    CONFIG_DFU_OVER_USB=y
    # CONFIG_DFU_TFTP is not set
    CONFIG_DFU_MMC=y
    CONFIG_DFU_RAM=y
    CONFIG_DFU_SF=y
    
    #
    # DMA Support
    #
    CONFIG_DMA=y
    CONFIG_DMA_CHANNELS=y
    # CONFIG_TI_EDMA3 is not set
    CONFIG_TI_K3_NAVSS_UDMA=y
    
    #
    # Fastboot support
    #
    CONFIG_FASTBOOT=y
    CONFIG_USB_FUNCTION_FASTBOOT=y
    CONFIG_UDP_FUNCTION_FASTBOOT=y
    CONFIG_FASTBOOT_BUF_ADDR=0x82000000
    CONFIG_FASTBOOT_BUF_SIZE=0x2F000000
    CONFIG_FASTBOOT_USB_DEV=0
    CONFIG_FASTBOOT_FLASH=y
    CONFIG_FASTBOOT_FLASH_MMC=y
    CONFIG_FASTBOOT_FLASH_MMC_DEV=0
    CONFIG_FASTBOOT_GPT_NAME="gpt"
    CONFIG_FASTBOOT_MBR_NAME="mbr"
    CONFIG_FASTBOOT_CMD_OEM_FORMAT=y
    CONFIG_FIRMWARE=y
    CONFIG_ARM_PSCI_FW=y
    CONFIG_TI_SCI_PROTOCOL=y
    
    #
    # FPGA support
    #
    # CONFIG_FPGA_ALTERA is not set
    # CONFIG_FPGA_SOCFPGA is not set
    # CONFIG_FPGA_XILINX is not set
    # CONFIG_FPGA_SPARTAN3 is not set
    
    #
    # GPIO Support
    #
    CONFIG_DM_GPIO=y
    # CONFIG_ALTERA_PIO is not set
    # CONFIG_DWAPB_GPIO is not set
    # CONFIG_AT91_GPIO is not set
    # CONFIG_ATMEL_PIO4 is not set
    CONFIG_DA8XX_GPIO=y
    # CONFIG_INTEL_BROADWELL_GPIO is not set
    # CONFIG_INTEL_ICH6_GPIO is not set
    # CONFIG_IMX_RGPIO2P is not set
    # CONFIG_HSDK_CREG_GPIO is not set
    # CONFIG_LPC32XX_GPIO is not set
    # CONFIG_MSM_GPIO is not set
    # CONFIG_MXC_GPIO is not set
    # CONFIG_CMD_PCA953X is not set
    # CONFIG_PCF8575_GPIO is not set
    # CONFIG_ROCKCHIP_GPIO is not set
    # CONFIG_XILINX_GPIO is not set
    # CONFIG_CMD_TCA642X is not set
    # CONFIG_TEGRA_GPIO is not set
    # CONFIG_TEGRA186_GPIO is not set
    # CONFIG_VYBRID_GPIO is not set
    # CONFIG_DM_74X164 is not set
    CONFIG_DM_PCA953X=y
    # CONFIG_MPC8XXX_GPIO is not set
    
    #
    # Hardware Spinlock Support
    #
    # CONFIG_DM_HWSPINLOCK is not set
    
    #
    # I2C support
    #
    CONFIG_DM_I2C=y
    # CONFIG_DM_I2C_COMPAT is not set
    CONFIG_I2C_SET_DEFAULT_BUS_NUM=y
    CONFIG_I2C_DEFAULT_BUS_NUMBER=0x0
    # CONFIG_DM_I2C_GPIO is not set
    # CONFIG_SYS_I2C_FSL is not set
    # CONFIG_SYS_I2C_CADENCE is not set
    # CONFIG_SYS_I2C_DW is not set
    # CONFIG_SYS_I2C_INTEL is not set
    # CONFIG_SYS_I2C_IMX_LPI2C is not set
    # CONFIG_SYS_I2C_MXC is not set
    CONFIG_SYS_I2C_OMAP24XX=y
    CONFIG_SYS_OMAP24_I2C_SLAVE=1
    CONFIG_SYS_OMAP24_I2C_SPEED=100000
    # CONFIG_SYS_I2C_ROCKCHIP is not set
    # CONFIG_SYS_I2C_MVTWSI is not set
    # CONFIG_SYS_I2C_IHS is not set
    # CONFIG_I2C_MUX is not set
    CONFIG_INPUT=y
    # CONFIG_SPL_INPUT is not set
    # CONFIG_DM_KEYBOARD is not set
    # CONFIG_SPL_DM_KEYBOARD is not set
    # CONFIG_CROS_EC_KEYB is not set
    # CONFIG_TWL4030_INPUT is not set
    
    #
    # LED Support
    #
    # CONFIG_LED is not set
    # CONFIG_SPL_LED is not set
    # CONFIG_LED_STATUS is not set
    
    #
    # Mailbox Controller Support
    #
    CONFIG_DM_MAILBOX=y
    CONFIG_K3_SEC_PROXY=y
    
    #
    # Memory Controller drivers
    #
    
    #
    # Multifunction device drivers
    #
    CONFIG_MISC=y
    # CONFIG_ALTERA_SYSID is not set
    # CONFIG_ATSHA204A is not set
    # CONFIG_ROCKCHIP_EFUSE is not set
    # CONFIG_VEXPRESS_CONFIG is not set
    # CONFIG_CROS_EC is not set
    # CONFIG_DS4510 is not set
    # CONFIG_FSL_SEC_MON is not set
    # CONFIG_MXC_OCOTP is not set
    # CONFIG_NUVOTON_NCT6102D is not set
    # CONFIG_PWRSEQ is not set
    # CONFIG_PCA9551_LED is not set
    # CONFIG_TWL4030_LED is not set
    # CONFIG_WINBOND_W83627 is not set
    # CONFIG_I2C_EEPROM is not set
    # CONFIG_SPL_I2C_EEPROM is not set
    CONFIG_ZYNQ_GEM_I2C_MAC_OFFSET=0x0
    # CONFIG_GDSYS_RXAUI_CTRL is not set
    # CONFIG_GDSYS_IOEP is not set
    # CONFIG_MPC83XX_SERDES is not set
    # CONFIG_FS_LOADER is not set
    # CONFIG_GDSYS_SOC is not set
    # CONFIG_IHS_FPGA is not set
    # CONFIG_ESM_K3 is not set
    # CONFIG_ESM_PMIC is not set
    
    #
    # MMC Host controller Support
    #
    CONFIG_MMC=y
    CONFIG_MMC_WRITE=y
    # CONFIG_MMC_BROKEN_CD is not set
    CONFIG_DM_MMC=y
    CONFIG_SPL_DM_MMC=y
    # CONFIG_ARM_PL180_MMCI is not set
    CONFIG_MMC_QUIRKS=y
    CONFIG_MMC_HW_PARTITIONING=y
    # CONFIG_SUPPORT_EMMC_RPMB is not set
    # CONFIG_SUPPORT_EMMC_BOOT is not set
    CONFIG_MMC_IO_VOLTAGE=y
    CONFIG_SPL_MMC_IO_VOLTAGE=y
    CONFIG_MMC_UHS_SUPPORT=y
    CONFIG_SPL_MMC_UHS_SUPPORT=y
    CONFIG_MMC_HS400_SUPPORT=y
    CONFIG_SPL_MMC_HS400_SUPPORT=y
    CONFIG_MMC_HS200_SUPPORT=y
    CONFIG_SPL_MMC_HS200_SUPPORT=y
    CONFIG_MMC_VERBOSE=y
    # CONFIG_MMC_TRACE is not set
    # CONFIG_SPL_MMC_TINY is not set
    # CONFIG_MMC_DW is not set
    # CONFIG_MMC_MXC is not set
    # CONFIG_MMC_PCI is not set
    # CONFIG_MMC_OMAP_HS is not set
    CONFIG_MMC_SDHCI=y
    # CONFIG_MMC_SDHCI_SDMA is not set
    CONFIG_MMC_SDHCI_ADMA=y
    CONFIG_SPL_MMC_SDHCI_ADMA=y
    # CONFIG_MMC_SDHCI_BCMSTB is not set
    # CONFIG_MMC_SDHCI_CADENCE is not set
    CONFIG_MMC_SDHCI_AM654=y
    # CONFIG_MMC_SDHCI_KONA is not set
    # CONFIG_MMC_SDHCI_MSM is not set
    # CONFIG_MMC_SDHCI_S5P is not set
    # CONFIG_MMC_SDHCI_SPEAR is not set
    # CONFIG_MMC_SDHCI_STI is not set
    # CONFIG_MMC_SDHCI_XENON is not set
    # CONFIG_MMC_SDHCI_TANGIER is not set
    # CONFIG_STM32_SDMMC2 is not set
    # CONFIG_FTSDC010 is not set
    # CONFIG_FSL_ESDHC is not set
    
    #
    # MTD Support
    #
    CONFIG_MTD_PARTITIONS=y
    CONFIG_MTD=y
    CONFIG_MTD_NOR_FLASH=y
    CONFIG_MTD_DEVICE=y
    CONFIG_FLASH_CFI_DRIVER=y
    CONFIG_CFI_FLASH=y
    CONFIG_SYS_FLASH_USE_BUFFER_WRITE=y
    CONFIG_FLASH_CFI_MTD=y
    # CONFIG_SYS_FLASH_PROTECTION is not set
    CONFIG_SYS_FLASH_CFI=y
    # CONFIG_ALTERA_QSPI is not set
    CONFIG_HBMC_AM654=y
    # CONFIG_NAND is not set
    # CONFIG_MTD_SPI_NAND is not set
    
    #
    # SPI Flash Support
    #
    CONFIG_DM_SPI_FLASH=y
    CONFIG_SPI_FLASH=y
    CONFIG_SPI_FLASH_SFDP_SUPPORT=y
    # CONFIG_SPI_FLASH_BAR is not set
    # CONFIG_SF_DUAL_FLASH is not set
    # CONFIG_SPI_FLASH_ATMEL is not set
    # CONFIG_SPI_FLASH_EON is not set
    # CONFIG_SPI_FLASH_GIGADEVICE is not set
    # CONFIG_SPI_FLASH_ISSI is not set
    # CONFIG_SPI_FLASH_MACRONIX is not set
    # CONFIG_SPI_FLASH_SPANSION is not set
    CONFIG_SPI_FLASH_STMICRO=y
    # CONFIG_SPI_FLASH_SST is not set
    # CONFIG_SPI_FLASH_WINBOND is not set
    # CONFIG_SPI_FLASH_XMC is not set
    # CONFIG_SPI_FLASH_USE_4K_SECTORS is not set
    # CONFIG_SPI_FLASH_DATAFLASH is not set
    CONFIG_SPI_FLASH_MTD=y
    
    #
    # UBI support
    #
    # CONFIG_CONFIG_UBI_SILENCE_MSG is not set
    CONFIG_MTD_UBI=y
    CONFIG_MTD_UBI_WL_THRESHOLD=4096
    CONFIG_MTD_UBI_BEB_LIMIT=20
    # CONFIG_MTD_UBI_FASTMAP is not set
    
    #
    # Multiplexer drivers
    #
    CONFIG_MULTIPLEXER=y
    CONFIG_MUX_MMIO=y
    # CONFIG_BITBANGMII is not set
    # CONFIG_MV88E6352_SWITCH is not set
    CONFIG_PHYLIB=y
    # CONFIG_PHY_ADDR_ENABLE is not set
    # CONFIG_B53_SWITCH is not set
    # CONFIG_MV88E61XX_SWITCH is not set
    # CONFIG_PHYLIB_10G is not set
    # CONFIG_PHY_AQUANTIA is not set
    # CONFIG_PHY_ATHEROS is not set
    # CONFIG_PHY_BROADCOM is not set
    # CONFIG_PHY_CORTINA is not set
    # CONFIG_PHY_DAVICOM is not set
    # CONFIG_PHY_ET1011C is not set
    # CONFIG_PHY_LXT is not set
    # CONFIG_PHY_MARVELL is not set
    # CONFIG_PHY_MESON_GXL is not set
    # CONFIG_PHY_MICREL is not set
    # CONFIG_PHY_MSCC is not set
    # CONFIG_PHY_NATSEMI is not set
    # CONFIG_PHY_REALTEK is not set
    # CONFIG_PHY_SMSC is not set
    # CONFIG_PHY_TERANETICS is not set
    CONFIG_PHY_TI=y
    # CONFIG_PHY_VITESSE is not set
    # CONFIG_PHY_XILINX is not set
    CONFIG_PHY_FIXED=y
    # CONFIG_FSL_PFE is not set
    CONFIG_DM_ETH=y
    CONFIG_NETDEVICES=y
    # CONFIG_PHY_GIGE is not set
    # CONFIG_ALTERA_TSE is not set
    # CONFIG_BCM_SF2_ETH is not set
    # CONFIG_DWC_ETH_QOS is not set
    # CONFIG_E1000 is not set
    # CONFIG_ETH_DESIGNWARE is not set
    # CONFIG_ETHOC is not set
    # CONFIG_FTMAC100 is not set
    # CONFIG_FTGMAC100 is not set
    # CONFIG_MACB is not set
    # CONFIG_RGMII is not set
    # CONFIG_MII is not set
    # CONFIG_RTL8139 is not set
    # CONFIG_RTL8169 is not set
    # CONFIG_SMC911X is not set
    # CONFIG_SUN7I_GMAC is not set
    # CONFIG_SUN4I_EMAC is not set
    # CONFIG_SUN8I_EMAC is not set
    # CONFIG_SH_ETHER is not set
    # CONFIG_DRIVER_TI_CPSW is not set
    # CONFIG_DRIVER_TI_EMAC is not set
    # CONFIG_DRIVER_TI_KEYSTONE_NET is not set
    CONFIG_TI_AM65_CPSW_NUSS=y
    # CONFIG_TI_AM64_ICSSG_PRUETH is not set
    # CONFIG_SYS_DPAA_QBMAN is not set
    # CONFIG_TSEC_ENET is not set
    # CONFIG_PCI is not set
    
    #
    # PHY Subsystem
    #
    CONFIG_PHY=y
    CONFIG_SPL_PHY=y
    # CONFIG_NOP_PHY is not set
    # CONFIG_SPL_NOP_PHY is not set
    # CONFIG_AM654_PHY is not set
    # CONFIG_MSM8916_USB_PHY is not set
    # CONFIG_OMAP_USB2_PHY is not set
    CONFIG_PHY_CADENCE_SIERRA=y
    CONFIG_PHY_J721E_WIZ=y
    # CONFIG_MVEBU_COMPHY_SUPPORT is not set
    
    #
    # Pin controllers
    #
    CONFIG_PINCTRL=y
    CONFIG_PINCTRL_FULL=y
    # CONFIG_PINCTRL_GENERIC is not set
    CONFIG_SPL_PINCTRL=y
    CONFIG_SPL_PINCTRL_FULL=y
    # CONFIG_SPL_PINCTRL_GENERIC is not set
    # CONFIG_PINCTRL_AT91 is not set
    # CONFIG_PINCTRL_AT91PIO4 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3036 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3128 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3188 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK322X is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3288 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3328 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3368 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RK3399 is not set
    # CONFIG_PINCTRL_ROCKCHIP_RV1108 is not set
    CONFIG_PINCTRL_SINGLE=y
    # CONFIG_PINCTRL_STM32 is not set
    
    #
    # Power
    #
    
    #
    # Power Domain Support
    #
    CONFIG_POWER_DOMAIN=y
    CONFIG_TI_SCI_POWER_DOMAIN=y
    CONFIG_DM_PMIC=y
    CONFIG_PMIC_CHILDREN=y
    CONFIG_SPL_PMIC_CHILDREN=y
    # CONFIG_PMIC_ACT8846 is not set
    # CONFIG_PMIC_AS3722 is not set
    # CONFIG_DM_PMIC_FAN53555 is not set
    # CONFIG_DM_PMIC_PFUZE100 is not set
    # CONFIG_DM_PMIC_MAX77686 is not set
    # CONFIG_DM_PMIC_MAX8998 is not set
    # CONFIG_DM_PMIC_MC34708 is not set
    # CONFIG_PMIC_MAX8997 is not set
    # CONFIG_PMIC_PM8916 is not set
    # CONFIG_PMIC_RK8XX is not set
    # CONFIG_PMIC_S2MPS11 is not set
    # CONFIG_DM_PMIC_SANDBOX is not set
    # CONFIG_PMIC_S5M8767 is not set
    # CONFIG_PMIC_RN5T567 is not set
    # CONFIG_PMIC_TPS65090 is not set
    CONFIG_PMIC_PALMAS=y
    # CONFIG_PMIC_LP873X is not set
    # CONFIG_PMIC_LP87565 is not set
    # CONFIG_POWER_MC34VR500 is not set
    # CONFIG_DM_PMIC_TPS65910 is not set
    # CONFIG_PMIC_STPMU1 is not set
    CONFIG_SPL_PMIC_PALMAS=y
    # CONFIG_SPL_PMIC_LP873X is not set
    # CONFIG_SPL_PMIC_LP87565 is not set
    # CONFIG_PMIC_TPS65941 is not set
    CONFIG_DM_REGULATOR=y
    CONFIG_SPL_DM_REGULATOR=y
    # CONFIG_REGULATOR_PWM is not set
    CONFIG_DM_REGULATOR_FIXED=y
    CONFIG_SPL_DM_REGULATOR_FIXED=y
    CONFIG_DM_REGULATOR_GPIO=y
    CONFIG_SPL_DM_REGULATOR_GPIO=y
    CONFIG_DM_REGULATOR_PALMAS=y
    # CONFIG_DM_REGULATOR_PBIAS is not set
    # CONFIG_DM_REGULATOR_TPS62360 is not set
    CONFIG_SPL_DM_REGULATOR_PALMAS=y
    # CONFIG_K3_AVS0 is not set
    # CONFIG_DM_PWM is not set
    # CONFIG_PWM_SANDBOX is not set
    # CONFIG_U_QE is not set
    CONFIG_RAM=y
    CONFIG_SPL_RAM=y
    # CONFIG_STM32_SDRAM is not set
    # CONFIG_MPC83XX_SDRAM is not set
    # CONFIG_K3_J721E_DDRSS is not set
    
    #
    # Remote Processor drivers
    #
    CONFIG_REMOTEPROC=y
    # CONFIG_K3_SYSTEM_CONTROLLER is not set
    # CONFIG_REMOTEPROC_TI_K3_ARM64 is not set
    CONFIG_REMOTEPROC_TI_K3_DSP=y
    CONFIG_REMOTEPROC_TI_K3_R5F=y
    
    #
    # Reset Controller Support
    #
    CONFIG_DM_RESET=y
    CONFIG_RESET_TI_SCI=y
    # CONFIG_RESET_DRA7 is not set
    
    #
    # Real Time Clock
    #
    # CONFIG_DM_RTC is not set
    # CONFIG_SPL_DM_RTC is not set
    # CONFIG_RTC_PL031 is not set
    # CONFIG_RTC_S35392A is not set
    # CONFIG_RTC_MC146818 is not set
    # CONFIG_RTC_M41T62 is not set
    CONFIG_SCSI=y
    CONFIG_DM_SCSI=y
    
    #
    # Serial drivers
    #
    CONFIG_BAUDRATE=115200
    CONFIG_REQUIRE_SERIAL_CONSOLE=y
    # CONFIG_SPECIFY_CONSOLE_INDEX is not set
    CONFIG_SERIAL_PRESENT=y
    CONFIG_SPL_SERIAL_PRESENT=y
    CONFIG_TPL_SERIAL_PRESENT=y
    CONFIG_DM_SERIAL=y
    # CONFIG_SERIAL_RX_BUFFER is not set
    # CONFIG_SERIAL_SEARCH_ALL is not set
    CONFIG_SPL_DM_SERIAL=y
    # CONFIG_TPL_DM_SERIAL is not set
    # CONFIG_DEBUG_UART_SKIP_INIT is not set
    # CONFIG_ALTERA_JTAG_UART is not set
    # CONFIG_ALTERA_UART is not set
    # CONFIG_ARC_SERIAL is not set
    # CONFIG_ATMEL_USART is not set
    # CONFIG_BCM6345_SERIAL is not set
    # CONFIG_FSL_LINFLEXUART is not set
    # CONFIG_FSL_LPUART is not set
    # CONFIG_MVEBU_A3700_UART is not set
    # CONFIG_NULLDEV_SERIAL is not set
    CONFIG_SYS_NS16550=y
    # CONFIG_PL01X_SERIAL is not set
    # CONFIG_MSM_SERIAL is not set
    CONFIG_OMAP_SERIAL=y
    # CONFIG_PXA_SERIAL is not set
    # CONFIG_SIFIVE_SERIAL is not set
    # CONFIG_MTK_SERIAL is not set
    # CONFIG_SMEM is not set
    
    #
    # Sound support
    #
    # CONFIG_SOUND is not set
    
    #
    # SOC (System On Chip) specific Drivers
    #
    CONFIG_SOC_TI=y
    CONFIG_TI_K3_NAVSS_RINGACC=y
    # CONFIG_TI_PRUSS is not set
    CONFIG_SPI=y
    CONFIG_DM_SPI=y
    CONFIG_SPI_MEM=y
    # CONFIG_ALTERA_SPI is not set
    # CONFIG_ATCSPI200_SPI is not set
    # CONFIG_ATMEL_SPI is not set
    # CONFIG_BCMSTB_SPI is not set
    CONFIG_CADENCE_QSPI=y
    # CONFIG_DESIGNWARE_SPI is not set
    # CONFIG_EXYNOS_SPI is not set
    # CONFIG_FSL_DSPI is not set
    # CONFIG_ICH_SPI is not set
    # CONFIG_MTK_QSPI is not set
    # CONFIG_MVEBU_A3700_SPI is not set
    # CONFIG_PL022_SPI is not set
    # CONFIG_ROCKCHIP_SPI is not set
    # CONFIG_SUN4I_SPI is not set
    # CONFIG_TEGRA114_SPI is not set
    # CONFIG_TEGRA20_SFLASH is not set
    # CONFIG_TEGRA20_SLINK is not set
    # CONFIG_TEGRA210_QSPI is not set
    # CONFIG_TI_QSPI is not set
    # CONFIG_XILINX_SPI is not set
    # CONFIG_SOFT_SPI is not set
    # CONFIG_CF_SPI is not set
    # CONFIG_FSL_ESPI is not set
    # CONFIG_FSL_QSPI is not set
    # CONFIG_SH_SPI is not set
    # CONFIG_SH_QSPI is not set
    # CONFIG_KIRKWOOD_SPI is not set
    # CONFIG_LPC32XX_SSP is not set
    # CONFIG_MPC8XXX_SPI is not set
    # CONFIG_MXC_SPI is not set
    # CONFIG_MXS_SPI is not set
    # CONFIG_OMAP3_SPI is not set
    
    #
    # SPMI support
    #
    # CONFIG_SPMI is not set
    
    #
    # System reset device drivers
    #
    CONFIG_SYSRESET=y
    # CONFIG_SYSRESET_GPIO is not set
    # CONFIG_SYSRESET_PSCI is not set
    CONFIG_SYSRESET_TI_SCI=y
    # CONFIG_SYSRESET_SYSCON is not set
    # CONFIG_SYSRESET_WATCHDOG is not set
    # CONFIG_SYSRESET_MCP83XX is not set
    # CONFIG_TEE is not set
    # CONFIG_OPTEE is not set
    # CONFIG_DM_THERMAL is not set
    
    #
    # Timer Support
    #
    # CONFIG_TIMER is not set
    
    #
    # TPM support
    #
    CONFIG_USB=y
    CONFIG_DM_USB=y
    CONFIG_SPL_DM_USB=y
    CONFIG_DM_USB_GADGET=y
    CONFIG_SPL_DM_USB_GADGET=y
    
    #
    # USB Host Controller Drivers
    #
    CONFIG_USB_HOST=y
    CONFIG_USB_XHCI_HCD=y
    # CONFIG_USB_XHCI_DWC3 is not set
    # CONFIG_USB_XHCI_DWC3_OF_SIMPLE is not set
    # CONFIG_USB_XHCI_PCI is not set
    # CONFIG_USB_XHCI_FSL is not set
    # CONFIG_USB_EHCI_HCD is not set
    # CONFIG_USB_OHCI_HCD is not set
    # CONFIG_USB_UHCI_HCD is not set
    # CONFIG_USB_DWC2 is not set
    CONFIG_USB_CDNS3=y
    CONFIG_USB_CDNS3_GADGET=y
    CONFIG_USB_CDNS3_HOST=y
    CONFIG_SPL_USB_CDNS3_GADGET=y
    CONFIG_USB_CDNS3_TI=y
    # CONFIG_USB_DWC3 is not set
    
    #
    # Legacy MUSB Support
    #
    # CONFIG_USB_MUSB_HCD is not set
    # CONFIG_USB_MUSB_UDC is not set
    
    #
    # MUSB Controller Driver
    #
    # CONFIG_USB_MUSB_HOST is not set
    # CONFIG_USB_MUSB_GADGET is not set
    # CONFIG_USB_MUSB_TI is not set
    # CONFIG_USB_MUSB_AM35X is not set
    # CONFIG_USB_MUSB_DSPS is not set
    # CONFIG_USB_MUSB_PIO_ONLY is not set
    
    #
    # USB Phy
    #
    # CONFIG_TWL4030_USB is not set
    # CONFIG_OMAP_USB_PHY is not set
    # CONFIG_ROCKCHIP_USB2_PHY is not set
    
    #
    # ULPI drivers
    #
    
    #
    # USB peripherals
    #
    CONFIG_USB_STORAGE=y
    # CONFIG_USB_KEYBOARD is not set
    CONFIG_USB_GADGET=y
    CONFIG_USB_GADGET_MANUFACTURER="Texas Instruments"
    CONFIG_USB_GADGET_VENDOR_NUM=0x0451
    CONFIG_USB_GADGET_PRODUCT_NUM=0x6163
    # CONFIG_USB_GADGET_ATMEL_USBA is not set
    # CONFIG_USB_GADGET_BCM_UDC_OTG_PHY is not set
    # CONFIG_USB_GADGET_DWC2_OTG is not set
    # CONFIG_CI_UDC is not set
    CONFIG_USB_GADGET_VBUS_DRAW=2
    CONFIG_USB_GADGET_DUALSPEED=y
    CONFIG_USB_GADGET_DOWNLOAD=y
    CONFIG_USB_FUNCTION_MASS_STORAGE=y
    # CONFIG_USB_FUNCTION_ROCKUSB is not set
    # CONFIG_USB_FUNCTION_SDP is not set
    # CONFIG_USB_FUNCTION_THOR is not set
    # CONFIG_USB_ETHER is not set
    # CONFIG_USB_HOST_ETHER is not set
    
    #
    # UFS Host Controller Support
    #
    CONFIG_UFS=y
    CONFIG_CADENCE_UFS=y
    CONFIG_TI_J721E_UFS=y
    
    #
    # Graphics support
    #
    # CONFIG_DM_VIDEO is not set
    # CONFIG_SYS_WHITE_ON_BLACK is not set
    # CONFIG_NO_FB_CLEAR is not set
    
    #
    # TrueType Fonts
    #
    # CONFIG_VIDEO_VESA is not set
    # CONFIG_VIDEO_LCD_ANX9804 is not set
    # CONFIG_VIDEO_LCD_SSD2828 is not set
    # CONFIG_VIDEO_MVEBU is not set
    # CONFIG_I2C_EDID is not set
    # CONFIG_DISPLAY is not set
    # CONFIG_VIDEO_TEGRA20 is not set
    # CONFIG_VIDEO_BRIDGE is not set
    # CONFIG_VIDEO is not set
    # CONFIG_LCD is not set
    # CONFIG_VIDEO_SIMPLE is not set
    # CONFIG_VIDEO_DT_SIMPLEFB is not set
    # CONFIG_OSD is not set
    
    #
    # VirtIO Drivers
    #
    # CONFIG_VIRTIO_MMIO is not set
    
    #
    # 1-Wire support
    #
    # CONFIG_W1 is not set
    
    #
    # 1-wire EEPROM support
    #
    # CONFIG_W1_EEPROM is not set
    
    #
    # Watchdog Timer Support
    #
    # CONFIG_WATCHDOG is not set
    # CONFIG_WATCHDOG_RESET_DISABLE is not set
    # CONFIG_BCM2835_WDT is not set
    # CONFIG_ULP_WATCHDOG is not set
    # CONFIG_WDT is not set
    # CONFIG_IMX_WATCHDOG is not set
    # CONFIG_PHYS_TO_BUS is not set
    
    #
    # File systems
    #
    # CONFIG_FS_BTRFS is not set
    # CONFIG_FS_CBFS is not set
    CONFIG_FS_EXT4=y
    CONFIG_EXT4_WRITE=y
    CONFIG_FS_FAT=y
    CONFIG_FAT_WRITE=y
    CONFIG_FS_FAT_MAX_CLUSTSIZE=65536
    # CONFIG_FS_JFFS2 is not set
    # CONFIG_UBIFS_SILENCE_MSG is not set
    # CONFIG_FS_CRAMFS is not set
    # CONFIG_YAFFS2 is not set
    
    #
    # Library routines
    #
    # CONFIG_BCH is not set
    # CONFIG_CC_OPTIMIZE_LIBS_FOR_SPEED is not set
    # CONFIG_DYNAMIC_CRC_TABLE is not set
    CONFIG_LIB_UUID=y
    CONFIG_PRINTF=y
    CONFIG_SPL_PRINTF=y
    CONFIG_SPRINTF=y
    CONFIG_SPL_SPRINTF=y
    CONFIG_STRTO=y
    CONFIG_SPL_STRTO=y
    CONFIG_IMAGE_SPARSE=y
    CONFIG_IMAGE_SPARSE_FILLBUF_SIZE=0x80000
    CONFIG_SYS_HZ=1000
    # CONFIG_USE_TINY_PRINTF is not set
    # CONFIG_PANIC_HANG is not set
    CONFIG_REGEX=y
    CONFIG_LIB_RAND=y
    # CONFIG_LIB_HW_RAND is not set
    # CONFIG_SPL_TINY_MEMSET is not set
    # CONFIG_TPL_TINY_MEMSET is not set
    CONFIG_RBTREE=y
    # CONFIG_BITREVERSE is not set
    # CONFIG_CMD_DHRYSTONE is not set
    
    #
    # Security support
    #
    # CONFIG_AES is not set
    # CONFIG_RSA is not set
    # CONFIG_TPM is not set
    # CONFIG_SPL_TPM is not set
    
    #
    # Android Verified Boot
    #
    # CONFIG_LIBAVB is not set
    
    #
    # Hashing Support
    #
    CONFIG_SHA1=y
    CONFIG_SHA256=y
    # CONFIG_SHA_HW_ACCEL is not set
    CONFIG_MD5=y
    
    #
    # Compression Support
    #
    # CONFIG_LZ4 is not set
    CONFIG_LZMA=y
    CONFIG_LZO=y
    # CONFIG_SPL_LZ4 is not set
    # CONFIG_SPL_LZO is not set
    # CONFIG_SPL_GZIP is not set
    # CONFIG_ERRNO_STR is not set
    CONFIG_HEXDUMP=y
    CONFIG_OF_LIBFDT=y
    CONFIG_OF_LIBFDT_OVERLAY=y
    CONFIG_SPL_OF_LIBFDT=y
    # CONFIG_TPL_OF_LIBFDT is not set
    
    #
    # System tables
    #
    CONFIG_GENERATE_SMBIOS_TABLE=y
    CONFIG_SMBIOS_MANUFACTURER="ti"
    CONFIG_EFI_LOADER=y
    CONFIG_EFI_UNICODE_CAPITALIZATION=y
    # CONFIG_EFI_LOADER_BOUNCE_BUFFER is not set
    CONFIG_OPTEE_TZDRAM_SIZE=0x0000000
    CONFIG_OPTEE_TZDRAM_BASE=0x00000000
    # CONFIG_UNIT_TEST is not set
    
    addr_fit=0x90000000
    arch=arm
    args_all=setenv optargs earlycon=ns16550a,mmio32,0x02800000 ${mtdparts}
    args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
    args_ufs=setenv devtype scsi;setenv bootpart 1:1;run ufs_finduuid;setenv bootargs console = ${console} ${optargs}root=PARTUUID=${uuid} rw roo1
    autoload=no
    baudrate=115200
    board=j721e
    board_name=j721e
    board_rev=E7
    board_serial=0112
    board_software_revision=01
    boot=mmc
    boot_fit=0
    boot_rprocs=if test ${dorprocboot} -eq 1 && test ${boot} = mmc; then rproc init;run boot_rprocs_mmc;fi;
    boot_rprocs_mmc=env set rproc_id;env set rproc_fw;for i in ${rproc_fw_binaries} ; do if test -z "${rproc_id}" ; then env set rproc_id $i;elsee
    bootargs=console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 vm.overcommit_ratio=5 vm.overcommit_memory=2 root=/dev/mmcblk0p1 ip=192.10
    bootcmd=setenv autoload no;ext4load mmc 0:1 0x82000000 /boot/Image;ext4load mmc 0:1 0x81200000 /boot/k3-j721e-common-proc-board.dtb;booti 0x80
    bootdelay=2
    bootdir=/boot
    bootenvfile=uEnv.txt
    bootpart=1:2
    bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
    console=ttyS2,115200n8
    cpu=armv8
    default_device_tree=k3-j721e-common-proc-board.dtb
    dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 1
    dfu_alt_info_mmc=boot part 1 1;rootfs part 1 2;tiboot3.bin fat 1 1;tispl.bin fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1;sysfw.itb fat 1 1
    dfu_alt_info_ospi=tiboot3.bin raw 0x0 0x080000;tispl.bin raw 0x080000 0x200000;u-boot.img raw 0x280000 0x400000;u-boot-env raw 0x680000 0x0200
    dfu_alt_info_ram=tispl.bin ram 0x80080000 0x100000;u-boot.img ram 0x81000000 0x100000
    dfu_bufsiz=0x20000
    dorprocboot=0
    envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run l;
    eth1addr=70:ff:76:1d:98:5a
    eth2addr=70:ff:76:1d:98:5b
    eth3addr=70:ff:76:1d:98:5c
    eth4addr=70:ff:76:1d:98:5d
    ethaddr=50:51:a9:fc:f4:92
    fdtaddr=0x82000000
    fdtcontroladdr=fdebbca8
    findfdt=setenv name_fdt ${default_device_tree};setenv fdtfile ${name_fdt}
    finduuid=part uuid mmc ${bootpart} uuid
    gatewayip=192.168.0.110
    get_fdt_mmc=load mmc ${bootpart} ${fdtaddr} ${bootdir}/${name_fdt}
    get_fdt_ufs=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    get_fit_mmc=load mmc ${bootpart} ${addr_fit} ${bootdir}/${name_fit}
    get_kern_mmc=load mmc ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
    get_kern_ufs=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
    get_overlay_mmc=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load mmc ${bootpart} ${overlayaddr} ${bootdir}/${;
    get_overlay_ufs=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load scsi ${bootpart} ${overlayaddr} ${bootdir}/$;
    get_overlaystring=for overlay in $name_overlays;do;setenv overlaystring ${overlaystring}'#'${overlay};done;
    importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
    init_mmc=run args_all args_mmc
    init_ufs=ufs init; scsi scan; run args_ufs
    ipaddr=192.168.0.100
    loadaddr=0x80080000
    loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
    loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
    loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
    mainr5f0_0fwname=/lib/firmware/j7-main-r5f0_0-fw
    mainr5f0_0loadaddr=88000000
    mcur5f0_0fwname=/lib/firmware/j7-mcu-r5f0_0-fw
    mcur5f0_0loadaddr=89000000
    mmcboot=mmc dev ${mmcdev}; devnum=${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; ;
    mmcdev=1
    mmcloados=if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_;
    mmcrootfstype=ext4 rootwait
    mtdids=nor0=47040000.spi.0,nor0=47034000.hyperbus
    mtdparts=mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(o)
    name_fit=fitImage
    name_kern=Image
    netmask=255.255.255.0
    overlayaddr=0x83000000
    partitions=name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
    rd_spec=-
    rproc_fw_binaries=3 /lib/firmware/j7-main-r5f0_1-fw 4 /lib/firmware/j7-main-r5f1_0-fw 5 /lib/firmware/j7-main-r5f1_1-fw 6 /lib/firmware/j7-c6 
    rproc_load_and_boot_one=if load mmc ${bootpart} $loadaddr ${rproc_fw}; then if rproc load ${rproc_id} ${loadaddr} ${filesize}; then rproc stai
    run_fit=bootm ${addr_fit}#${fdtfile}${overlaystring}
    run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
    scsirootfstype=ext4 rootwait
    serial#=0000000000000112
    serverip=192.168.0.110
    soc=k3
    stderr=serial@2800000
    stdin=serial@2800000
    stdout=serial@2800000
    ufs_finduuid=part uuid scsi ${bootpart} uuid
    update_to_fit=setenv loadaddr ${addr_fit}; setenv bootfile ${name_fit}
    vendor=ti
    
    u-boot-env.txt

  • Hi Keerthy,

    Is there any update on this issue.

    Please let me know if any information is needed.

    Regards,

    Sainath

  • Hi Sainath,

    I believe you are on SDK 6.02 and i am yet to have the older setup. The latest
    release is 7.0. So i will revert back in a day or two.


    - Keerthy

  • Hi,

    Thank you for the reply.

    The current SDK version which is being used is 7.02.

    Thank you.

    Regards,

    Sainath

  • Hi Sainath,

    I wonder why mybootconfig file that you attached shows 2019.01 which is older SDK.

    "

    #
    # Automatically generated file; DO NOT EDIT.
    # U-Boot 2019.01 Configuration"

    Could you please double confirm on that before i try to reproduce at my end?

    Best Regards,
    Keerthy

  • Hi,

    Sorry about that.

    I am using SDK 7.02. But, the Uboot is downloaded from below link and built it manually:

    git clone -b processor-sdk-u-boot-2019.01 git://git.ti.com/processor-sdk/processor-sdk-u-boot.git 

    But, the root file system belongs to SDK 7.02.

    Do I need to use latest Uboot source code.

    Thanks again.

  • Sainath,

    The 7.02 SDK comes with its own u-boot(2020 Based) can you please try with that? 2019.01 is older
    branch.

    Best Regards,
    Keerthy