Hi,
I am working on jacinto 6 with android on it.It worked fine but now when I start the board it is rebooting continously, I tried to flash android images on to the board thinking it is a android issue but the device is not detected to flash the images.
Here is the dmesg log while the board is booted up.
[ 5.768557] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: (null)
[ 5.768672] init: [libfs_mgr]__mount(source=/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache,target=/cache,type=ext4)=0
[ 5.769634] init: [libfs_mgr]superblock s_max_mnt_count:10,/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata
[ 5.769658] init: [libfs_mgr]do_quota_with_shutdown_check(): was not clealy shutdown, state flag:1incompat flag:46
[ 5.769677] init: [libfs_mgr]Requested quota status is match on /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata
[ 5.770096] EXT4-fs (mmcblk0p17): Ignoring removed nomblk_io_submit option
[ 5.873828] ti_oppdm 4a003b20.oppdm: vdd failed for voltage 1070000uV(ref=1060000uV)[min 850000uV max 1500000uV]:-121
[ 5.884506] cpufreq: __target_index: Failed to change cpu frequency: -121
[ 5.891619] ti_oppdm 4a003b20.oppdm: vdd failed for voltage 1185000uV(ref=1210000uV)[min 950000uV max 1500000uV]:-121
[ 5.902540] ti_oppdm 4a003b20.oppdm: vdd failed for voltage 1070000uV(ref=1060000uV)[min 850000uV max 1500000uV]:-121
[ 5.913208] cpufreq: __target_index: Failed to change cpu frequency: -121
Please suggest me the solution for the issue.
With Regards,
-Vamsi