Part Number: PROCESSOR-SDK-AM437X
Hello,
I have been trying to use the "ip" command to configure the CAN interface. When executed:
ip link set can0 type can bitrate 125000
Response:
ip: either "dev" is duplicate, or "type" is garbage
I have visited threads which mention missing iproute2. In particular:
When following the resolution in the above thread, I found the relevant sections missing.
What should I do to configure and use the CAN bus?
Thanks,
Peiman