This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3356: Uniflash Error

Part Number: AM3356
Other Parts Discussed in Thread: UNIFLASH,

Hi,

Our customer is trying to write Flash via JTAG with Uniflash.
I am consulting by saying that an error occurs at this time.
I've never used Uniflash, so I'm not sure.
The execution log is as follows.

----------------------------------------------------------------------------------------------------

c:\ti\uniflash_5.2.0>C:\ti\uniflash_5.2.0\dslite.bat --mode load --config = C:\Users\xxxxx.xxx\ti\CCSTargetConfigurations\XDS110_am335x.ccxml -f C:\ti\uniflash_5.2.0\processors\FlashWriter\evmAM335x\uart_evmAM335x_flash_programmer.out -n 8 Executing the following command:
> "C:\ti\uniflash_5.2.0\deskdb\content\TICloudAgent\win\ccs_base\DebugSe
> rver\bin\DSLite" load --config =
> C:\Users\xxxxx.xxx\ti\CCSTargetConfigurations\XDS110_am335x.ccx
> ml -f
> C:\ti\uniflash_5.2.0\processors\FlashWriter\evmAM335x\uart_evmAM335x_f
> lash_programmer.out -n 8

For more details and examples, please refer to the UniFlash Quick Start guide.

DSLite version 10.0.0.1942
Configuring Debugger (may take a few minutes on first launch)...
Failed: Cannot read System Setup data from XML file c:\ti\uniflash_5.2.0\= Error parsing file:
Fatal Error at (0, 0): An exception occurred! Type:RuntimeException, Message:The primary document entity could not be opened. Id=c:\ti\uniflash_5.2.0\=

----------------------------------------------------------------------------------------------------

The question from them is
1. How to avoid the error
2. What should be specified in <Core ID to be Connected to JTAG on the Target Platform> of AM3356?

Can you give me any advice?

Best Regards,

Kouji Nishigata