I modified the encode demo on DM6467T evaluation board to use h264fhdenc. The load on the DSP was about 95% and the display flickered from time to time, especially noticeable on the red color. When I used 720p video or reduced the frame rate to the encoder to 20 fps, I did not see any flickers. Have anyone experience the same problem? How can I fix this? Thank you.