Part Number: TDA4VM
If I have 2 phys that interface to the MAIN domain on TDA4VM in RMII mode. Each PHY has an output reference clock for TX and RX. Note that the TDA4 has only one clock reference input in the main domain. What do I need to do in regards to the second reference clock from the second RMII PHY if they both need to be connected to the MAIN domain?