This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730:Advisory 1.40 HS USB OTG Software Reset Is Not Fully Functional

Guru 10095 points

Hello.
I would like to make sure about the Work around of Advisory 1.40.
Do ULPI RegAddr and ULPI RegData registers in the Work around
mean Register INSNREG05_ULPI?
If so, what value should be set the register to reset?

Advisory 1.40 HS USB OTG Software Reset Is Not Fully Functional
Workaround(s) Use the ULPI RegAddr and ULPI RegData registers to manually
send the reset command to the PHY. As soon as this is done, LINK and PHY
can begin negotiating and functioning normally.

Regards,
Kanae