This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VMXEVM: Trying to load binaries with 0

Part Number: TDA4VMXEVM


Hi,

We followed the instruction to load binaries on target to the TDAx4 EVM.
In section 6.4:
https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/latest/exports/docs/psdk_rtos_auto/docs/user_guide/ccs_setup_j721e.html#step-2-setup-ccs-target-configuration-and-gels-files

we are running the 'LoadJsFile' as described in figure 6.5 we get the following message:

Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 8.4.0.00006)

Why is that?

Is there any other way to load binaries?
Do we must purchase that XDS110 device? 
Are the supplied drivers not support a PC USB to XDS110/Emulator direct cable connection?