Part Number: DM3730
I see conflicting information on whether this interface is supported on the DM3730CBPA, was hoping to get clarification. The AM-DM37x Multimedia Device TRM, table 1-3 shows it does not support it for the CBPA package, and states that even though the TRM talks about the interface it might not be available, referring you to table 1-3 for clarification. The datasheet for the dm3730 on page31 & in table 2.4 shows the ball name AG17 and the available functions that can be routed to that ball: cam_d0, gpio_99 and save_mode. No mention of CSI2. So it would seem like it's not available. However other postings have said the table 1-3 is incorrect. Is there an updated document that indicates that, as well as how to properly configure the pin mapping to enable that feature? If it is supported can you also clarify the number of lanes supported?