This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: Customer PCB using AM437 cannot boot, needs MLO/SBL dump to debug

Part Number: AM4378

Hi Champs:

The customer is using the AM437 for making their PCB within SDK6.

Due to the boot SD card cannot be successful, and the console shows nothing,

However, if we used the SDK2.0 (2015 version) , the console shows something, so we need to open the Dump log in MLO/SBL/uBoot in SDK6/7.

Can you tell us how to open the log in MLO/SBL for debugging this?

THanks.

BR Rio

  • Hello Rio,

    To confirm, are they using SDK6 from multiple years ago? Or are you talking about Linux Processor SDK 6.1/6.3 from December 2019 / March 2020? Please note that on the forums, we do not support Linux software releases that are older than about 2 years.

    Regards,

    Nick

  • Hi Nick:

    -->Processor SDK 6.1/6.3 from December 2019 / March 2020

    I'm talking about the SDK released on 2019.

    Below is my working path, you can see the git version is 2019.

    /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a

    THanks.

    BR Rio

  • Hi Rio,

    Will you check SPL/u-boot bring-up tips as outlined in the link below:

    software-dl.ti.com/.../U-Boot.html

    Best,

    -Hong

  • Hi Hong:

    May you guide me how to solve this build error?

    THanks.

    BR Rio

    /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-ld.bfd: common/spl/built-in.o: in function `preloader_console_init':
    /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a/common/spl/spl.c:712: undefined reference to `spl_display_print'
    scripts/Makefile.spl:377: recipe for target 'spl/u-boot-spl' failed
    make[1]: *** [spl/u-boot-spl] Error 1
    Makefile:1662: recipe for target 'spl/u-boot-spl' failed
    make: *** [spl/u-boot-spl] Error 2
    make: Leaving directory '/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a'
    copy MLO to am43xx_evm
    copy u-boot.img to am43xx_evm

  • /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-ld.bfd: common/built-in.o:(.rodata.init_sequence_f+0x2c): undefined reference to `board_early_init_f'
    /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-ld.bfd: common/built-in.o:(.data.init_sequence_r+0x6c): undefined reference to `misc_init_r'
    Makefile:1504: recipe for target 'u-boot' failed
    make: *** [u-boot] Error 1
    make: Leaving directory '/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a'
    copy MLO to am43xx_evm
    copy u-boot.img to am43xx_evm
    root@ubuntu:/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a#

    Hi Champs:

    Now, I have those 2 errors while building SPL.

    Please help.

    THanks.

    BR Rio

  • Hi Rio,

    1. Have you referred the link when launching u-boot build?

    https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/AM437X/linux/Foundational_Components_U-Boot.html#build-and-boot-flow-on-32-bit-platforms

    2. On your original question “Can you tell us how to open the log in MLO/SBL for debugging this?”

    Depending on the board bring-up issue you want to debug on, there’re options to “use JTAG debugger” or “enable early serial dump”

    I’m listing an example SPL boot flow below, It shows that “normal serial dump” is bit late in reference to board configuration, i.e. DDR configuration in this example.

    There’s a link on how to enable early serial dump in SPL.

    https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/AM437X/linux/How_to_Guides/Board_Port/U-Boot.html#u-boot-bringup-debugging-tips 

    >>>> example SPL boot flow

    main (asm){

    a)      …

    b)      board_init_f() -> sdram_init() -> config_ddr()

    c)       board_init_r() -> spl_board_init() -> preloader_console_init() -> serial_init() -> puts(“xyz”)

    d)      …

    Best,

    -Hong

  • Hi Hong:

     

    #1. The 2 compile errors are solved, due to I add some new configs for spl_display_print + misc_init_r.

          I think those 2 configs should be helpful for allowing me showing something while MLO/SPL stage. However, AM43xx is not able to add those 2 configs.

          So, I remove them for solving this.

     

    #2. May you help me to review my am43xx_evm_defconfig in the attached. 

          I still have nothing to show on the customer UART console L.  

     ((Sorry, I cannot not upload the deconfig onto E2E, not knowing why, you can find it in the mail I sent to you).

    Any comments?

     

    BR Rio

  • Hi Rio,

    1. It is good to know your build error got fixed.
    2. For your reference, I’m attaching the patch I used for adding early UART in SPL on AM437x GP EVM, where I used the latest SDK 6.3 as a baseline.

    The UART dump is listed below, where yellow highlighted one are newly added UART dump.

    <debug_uart>

    Passed early_system_init()

    Passed board_early_init_f()

    Passed sdram_init()

    U-Boot SPL 2019.01-gbf025b2599-dirty (Aug 14 2020 - 08:14:04 -0500)

    Trying to boot from MMC1 

    Best,

    -Hong

    From 60bbdb6643c170a4e5da07164492f19e6ccee5ab Mon Sep 17 00:00:00 2001
    From: [Hong Guan] <hguan@ti.com>
    Date: Thu, 13 Aug 2020 17:18:24 -0700
    Subject: [PATCH 1/1] SDK6.3 early UART print enable in SPL with printf example


    Signed-off-by: [Hong Guan] <hguan@ti.com>
    ---
    arch/arm/mach-omap2/am33xx/board.c | 3 +++
    configs/am43xx_evm_defconfig | 7 +++++++
    2 files changed, 10 insertions(+), 0 deletions(-)
    mode change 100644 => 100755 arch/arm/mach-omap2/am33xx/board.c
    mode change 100644 => 100755 configs/am43xx_evm_defconfig

    diff --git a/arch/arm/mach-omap2/am33xx/board.c b/arch/arm/mach-omap2/am33xx/board.c
    old mode 100644
    new mode 100755
    index 62158a9..051a2b8
    --- a/arch/arm/mach-omap2/am33xx/board.c
    +++ b/arch/arm/mach-omap2/am33xx/board.c
    @@ -534,8 +534,11 @@ void board_init_f(ulong dummy)
    {
    hw_data_init();
    early_system_init();
    + printf("\nPassed early_system_init()\n");
    board_early_init_f();
    + printf("\nPassed board_early_init_f()\n");
    sdram_init();
    + printf("\nPassed sdram_init()\n");
    /* dram_init must store complete ramsize in gd->ram_size */
    gd->ram_size = get_ram_size(
    (void *)CONFIG_SYS_SDRAM_BASE,
    diff --git a/configs/am43xx_evm_defconfig b/configs/am43xx_evm_defconfig
    old mode 100644
    new mode 100755
    index 6272063..6b7afb0
    --- a/configs/am43xx_evm_defconfig
    +++ b/configs/am43xx_evm_defconfig
    @@ -12,6 +12,13 @@ CONFIG_SYS_EXTRA_OPTIONS="CONS_INDEX=1"
    CONFIG_SYS_CONSOLE_INFO_QUIET=y
    # CONFIG_MISC_INIT_R is not set
    CONFIG_VERSION_VARIABLE=y
    +# early UART
    +CONFIG_DEBUG_UART_BASE=0x44e09000
    +CONFIG_DEBUG_UART_CLOCK=48000000
    +CONFIG_DEBUG_UART=y
    +CONFIG_DEBUG_UART_OMAP=y
    +CONFIG_DEBUG_UART_SHIFT=2
    +CONFIG_DEBUG_UART_ANNOUNCE=y
    CONFIG_SPL_ETH_SUPPORT=y
    CONFIG_SPL_MTD_SUPPORT=y
    CONFIG_SPL_NET_SUPPORT=y
    -- 
    1.7.1



  • Hi Rio, 

    The following line is common for TI EVMs: GP EVM (2GB DDR), IDK/SK EVM (1GB DDR).

    ./include/configs/am43xx_evm.h:#define CONFIG_MAX_RAM_BANK_SIZE               (1024 << 21)        /* 2GB */

    But the actual DDR size is run-time detected and passed to GD structure in get_ram_size() call as listed below; 

    In fact, get_ram_size() is one of quick, but effective memory testing after DDR configuration, and strongly recommended when porting u-boot.

    For your failing case of code trapping in get_ram_size() call,  I would look into DDR configuration in sdram_init().

    board_init_f()
    {
    	…
    	sdram_init();
    	printf("\nPassed sdram_init()\n");
    	/* dram_init must store complete ramsize in gd->ram_size */
    	gd->ram_size = get_ram_size(
    			(void *)CONFIG_SYS_SDRAM_BASE,
    			CONFIG_MAX_RAM_BANK_SIZE);
    	…
    }
    
    /*
     * Check memory range for valid RAM. A simple memory test determines
     * the actually available RAM size between addresses `base' and
     * `base + maxsize'.
     */
    long get_ram_size(long *base, long maxsize)

    Best,

    -Hong

  • Hi Hong:

    May you review my board_f.c which has the board_init_f function inside?

    It cannot take the patch you pointed here :(.

    Thanks.

    // SPDX-License-Identifier: GPL-2.0+
    /*
     * Copyright (c) 2011 The Chromium OS Authors.
     * (C) Copyright 2002-2006
     * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
     *
     * (C) Copyright 2002
     * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
     * Marius Groeger <mgroeger@sysgo.de>
     */
    
    #include <common.h>
    #include <bloblist.h>
    #include <console.h>
    #include <cpu.h>
    #include <dm.h>
    #include <environment.h>
    #include <fdtdec.h>
    #include <fs.h>
    #include <i2c.h>
    #include <initcall.h>
    #include <malloc.h>
    #include <mapmem.h>
    #include <os.h>
    #include <post.h>
    #include <relocate.h>
    #ifdef CONFIG_SPL
    #include <spl.h>
    #endif
    #include <status_led.h>
    #include <sysreset.h>
    #include <timer.h>
    #include <trace.h>
    #include <video.h>
    #include <watchdog.h>
    #ifdef CONFIG_MACH_TYPE
    #include <asm/mach-types.h>
    #endif
    #if defined(CONFIG_MP) && defined(CONFIG_PPC)
    #include <asm/mp.h>
    #endif
    #include <asm/io.h>
    #include <asm/sections.h>
    #include <dm/root.h>
    #include <linux/errno.h>
    
    /*
     * Pointer to initial global data area
     *
     * Here we initialize it if needed.
     */
    #ifdef XTRN_DECLARE_GLOBAL_DATA_PTR
    #undef	XTRN_DECLARE_GLOBAL_DATA_PTR
    #define XTRN_DECLARE_GLOBAL_DATA_PTR	/* empty = allocate here */
    DECLARE_GLOBAL_DATA_PTR = (gd_t *)(CONFIG_SYS_INIT_GD_ADDR);
    #else
    DECLARE_GLOBAL_DATA_PTR;
    #endif
    
    /*
     * TODO(sjg@chromium.org): IMO this code should be
     * refactored to a single function, something like:
     *
     * void led_set_state(enum led_colour_t colour, int on);
     */
    /************************************************************************
     * Coloured LED functionality
     ************************************************************************
     * May be supplied by boards if desired
     */
    __weak void coloured_LED_init(void) {}
    __weak void red_led_on(void) {}
    __weak void red_led_off(void) {}
    __weak void green_led_on(void) {}
    __weak void green_led_off(void) {}
    __weak void yellow_led_on(void) {}
    __weak void yellow_led_off(void) {}
    __weak void blue_led_on(void) {}
    __weak void blue_led_off(void) {}
    
    /*
     * Why is gd allocated a register? Prior to reloc it might be better to
     * just pass it around to each function in this file?
     *
     * After reloc one could argue that it is hardly used and doesn't need
     * to be in a register. Or if it is it should perhaps hold pointers to all
     * global data for all modules, so that post-reloc we can avoid the massive
     * literal pool we get on ARM. Or perhaps just encourage each module to use
     * a structure...
     */
    
    #if defined(CONFIG_WATCHDOG) || defined(CONFIG_HW_WATCHDOG)
    static int init_func_watchdog_init(void)
    {
    # if defined(CONFIG_HW_WATCHDOG) && \
    	(defined(CONFIG_M68K) || defined(CONFIG_MICROBLAZE) || \
    	defined(CONFIG_SH) || \
    	defined(CONFIG_DESIGNWARE_WATCHDOG) || \
    	defined(CONFIG_IMX_WATCHDOG))
    	hw_watchdog_init();
    	puts("       Watchdog enabled\n");
    # endif
    	WATCHDOG_RESET();
    
    	return 0;
    }
    
    int init_func_watchdog_reset(void)
    {
    	WATCHDOG_RESET();
    
    	return 0;
    }
    #endif /* CONFIG_WATCHDOG */
    
    __weak void board_add_ram_info(int use_default)
    {
    	/* please define platform specific board_add_ram_info() */
    }
    
    static int init_baud_rate(void)
    {
    	gd->baudrate = env_get_ulong("baudrate", 10, CONFIG_BAUDRATE);
    	return 0;
    }
    
    static int display_text_info(void)
    {
    #if !defined(CONFIG_SANDBOX) && !defined(CONFIG_EFI_APP)
    	ulong bss_start, bss_end, text_base;
    
    	bss_start = (ulong)&__bss_start;
    	bss_end = (ulong)&__bss_end;
    
    #ifdef CONFIG_SYS_TEXT_BASE
    	text_base = CONFIG_SYS_TEXT_BASE;
    #else
    	text_base = CONFIG_SYS_MONITOR_BASE;
    #endif
    
    	printf("U-Boot code: %08lX -> %08lX  BSS: -> %08lX\n",
    	      text_base, bss_start, bss_end);
    #endif
    
    	return 0;
    }
    
    #ifdef CONFIG_SYSRESET
    static int print_resetinfo(void)
    {
    	struct udevice *dev;
    	char status[256];
    	int ret;
    
    	ret = uclass_first_device_err(UCLASS_SYSRESET, &dev);
    	if (ret) {
    		printf("%s: No sysreset device found (error: %d)\n",
    		      __func__, ret);
    		/* Not all boards have sysreset drivers available during early
    		 * boot, so don't fail if one can't be found.
    		 */
    		return 0;
    	}
    
    	if (!sysreset_get_status(dev, status, sizeof(status)))
    		printf("%s", status);
    
    	return 0;
    }
    #endif
    
    #if defined(CONFIG_DISPLAY_CPUINFO) && CONFIG_IS_ENABLED(CPU)
    static int print_cpuinfo(void)
    {
    	struct udevice *dev;
    	char desc[512];
    	int ret;
    
    	ret = uclass_first_device_err(UCLASS_CPU, &dev);
    	if (ret) {
    		printf("%s: Could not get CPU device (err = %d)\n",
    		      __func__, ret);
    		return ret;
    	}
    
    	ret = cpu_get_desc(dev, desc, sizeof(desc));
    	if (ret) {
    		printf("%s: Could not get CPU description (err = %d)\n",
    		      dev->name, ret);
    		return ret;
    	}
    
    	printf("CPU:   %s\n", desc);
    
    	return 0;
    }
    #endif
    
    static int announce_dram_init(void)
    {
    	puts("DRAM:  ");
    	return 0;
    }
    
    static int show_dram_config(void)
    {
    	unsigned long long size;
    
    #ifdef CONFIG_NR_DRAM_BANKS
    	int i;
    
    	printf("\nRAM Configuration:\n");
    	for (i = size = 0; i < CONFIG_NR_DRAM_BANKS; i++) {
    		size += gd->bd->bi_dram[i].size;
    		printf("Bank #%d: %llx ", i,
    		      (unsigned long long)(gd->bd->bi_dram[i].start));
    #ifdef printf
    		print_size(gd->bd->bi_dram[i].size, "\n");
    #endif
    	}
    	printf("\nDRAM:  ");
    #else
    	size = gd->ram_size;
    #endif
    
    	print_size(size, "");
    	board_add_ram_info(0);
    	putc('\n');
    
    	return 0;
    }
    
    __weak int dram_init_banksize(void)
    {
    #if defined(CONFIG_NR_DRAM_BANKS) && defined(CONFIG_SYS_SDRAM_BASE)
    	gd->bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
    	gd->bd->bi_dram[0].size = get_effective_memsize();
    #endif
    
    	return 0;
    }
    
    #if defined(CONFIG_SYS_I2C)
    static int init_func_i2c(void)
    {
    	puts("I2C:   ");
    #ifdef CONFIG_SYS_I2C
    	i2c_init_all();
    #else
    	i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
    #endif
    	puts("ready\n");
    	return 0;
    }
    #endif
    
    #if defined(CONFIG_VID)
    __weak int init_func_vid(void)
    {
    	return 0;
    }
    #endif
    
    static int setup_mon_len(void)
    {
    #if defined(__ARM__) || defined(__MICROBLAZE__)
    	gd->mon_len = (ulong)&__bss_end - (ulong)_start;
    #elif defined(CONFIG_SANDBOX) || defined(CONFIG_EFI_APP)
    	gd->mon_len = (ulong)&_end - (ulong)_init;
    #elif defined(CONFIG_NIOS2) || defined(CONFIG_XTENSA)
    	gd->mon_len = CONFIG_SYS_MONITOR_LEN;
    #elif defined(CONFIG_NDS32) || defined(CONFIG_SH) || defined(CONFIG_RISCV)
    	gd->mon_len = (ulong)(&__bss_end) - (ulong)(&_start);
    #elif defined(CONFIG_SYS_MONITOR_BASE)
    	/* TODO: use (ulong)&__bss_end - (ulong)&__text_start; ? */
    	gd->mon_len = (ulong)&__bss_end - CONFIG_SYS_MONITOR_BASE;
    #endif
    	return 0;
    }
    
    static int setup_spl_handoff(void)
    {
    #if CONFIG_IS_ENABLED(HANDOFF)
    	gd->spl_handoff = bloblist_find(BLOBLISTT_SPL_HANDOFF,
    					sizeof(struct spl_handoff));
    	printf("Found SPL hand-off info %p\n", gd->spl_handoff);
    #endif
    
    	return 0;
    }
    
    __weak int arch_cpu_init(void)
    {
    	return 0;
    }
    
    __weak int mach_cpu_init(void)
    {
    	return 0;
    }
    
    /* Get the top of usable RAM */
    __weak ulong board_get_usable_ram_top(ulong total_size)
    {
    #ifdef CONFIG_SYS_SDRAM_BASE
    	/*
    	 * Detect whether we have so much RAM that it goes past the end of our
    	 * 32-bit address space. If so, clip the usable RAM so it doesn't.
    	 */
    	if (gd->ram_top < CONFIG_SYS_SDRAM_BASE)
    		/*
    		 * Will wrap back to top of 32-bit space when reservations
    		 * are made.
    		 */
    		return 0;
    #endif
    	return gd->ram_top;
    }
    
    static int setup_dest_addr(void)
    {
    	printf("Monitor len: %08lX\n", gd->mon_len);
    	/*
    	 * Ram is setup, size stored in gd !!
    	 */
    	printf("Ram size: %08lX\n", (ulong)gd->ram_size);
    #if defined(CONFIG_SYS_MEM_TOP_HIDE)
    	/*
    	 * Subtract specified amount of memory to hide so that it won't
    	 * get "touched" at all by U-Boot. By fixing up gd->ram_size
    	 * the Linux kernel should now get passed the now "corrected"
    	 * memory size and won't touch it either. This should work
    	 * for arch/ppc and arch/powerpc. Only Linux board ports in
    	 * arch/powerpc with bootwrapper support, that recalculate the
    	 * memory size from the SDRAM controller setup will have to
    	 * get fixed.
    	 */
    	gd->ram_size -= CONFIG_SYS_MEM_TOP_HIDE;
    #endif
    #ifdef CONFIG_SYS_SDRAM_BASE
    	gd->ram_base = CONFIG_SYS_SDRAM_BASE;
    #endif
    	gd->ram_top = gd->ram_base + get_effective_memsize();
    	gd->ram_top = board_get_usable_ram_top(gd->mon_len);
    	gd->relocaddr = gd->ram_top;
    	printf("Ram top: %08lX\n", (ulong)gd->ram_top);
    #if defined(CONFIG_MP) && (defined(CONFIG_MPC86xx) || defined(CONFIG_E500))
    	/*
    	 * We need to make sure the location we intend to put secondary core
    	 * boot code is reserved and not used by any part of u-boot
    	 */
    	if (gd->relocaddr > determine_mp_bootpg(NULL)) {
    		gd->relocaddr = determine_mp_bootpg(NULL);
    		printf("Reserving MP boot page to %08lx\n", gd->relocaddr);
    	}
    #endif
    	return 0;
    }
    
    #ifdef CONFIG_PRAM
    /* reserve protected RAM */
    static int reserve_pram(void)
    {
    	ulong reg;
    
    	reg = env_get_ulong("pram", 10, CONFIG_PRAM);
    	gd->relocaddr -= (reg << 10);		/* size is in kB */
    	printf("Reserving %ldk for protected RAM at %08lx\n", reg,
    	      gd->relocaddr);
    	return 0;
    }
    #endif /* CONFIG_PRAM */
    
    /* Round memory pointer down to next 4 kB limit */
    static int reserve_round_4k(void)
    {
    	gd->relocaddr &= ~(4096 - 1);
    	return 0;
    }
    
    #ifdef CONFIG_ARM
    __weak int reserve_mmu(void)
    {
    #if !(defined(CONFIG_SYS_ICACHE_OFF) && defined(CONFIG_SYS_DCACHE_OFF))
    	/* reserve TLB table */
    	gd->arch.tlb_size = PGTABLE_SIZE;
    	gd->relocaddr -= gd->arch.tlb_size;
    
    	/* round down to next 64 kB limit */
    	gd->relocaddr &= ~(0x10000 - 1);
    
    	gd->arch.tlb_addr = gd->relocaddr;
    	printf("TLB table from %08lx to %08lx\n", gd->arch.tlb_addr,
    	      gd->arch.tlb_addr + gd->arch.tlb_size);
    
    #ifdef CONFIG_SYS_MEM_RESERVE_SECURE
    	/*
    	 * Record allocated tlb_addr in case gd->tlb_addr to be overwritten
    	 * with location within secure ram.
    	 */
    	gd->arch.tlb_allocated = gd->arch.tlb_addr;
    #endif
    #endif
    
    	return 0;
    }
    #endif
    
    static int reserve_video(void)
    {
    #ifdef CONFIG_DM_VIDEO
    	ulong addr;
    	int ret;
    
    	addr = gd->relocaddr;
    	ret = video_reserve(&addr);
    	if (ret)
    		return ret;
    	gd->relocaddr = addr;
    #elif defined(CONFIG_LCD)
    #  ifdef CONFIG_FB_ADDR
    	gd->fb_base = CONFIG_FB_ADDR;
    #  else
    	/* reserve memory for LCD display (always full pages) */
    	gd->relocaddr = lcd_setmem(gd->relocaddr);
    	gd->fb_base = gd->relocaddr;
    #  endif /* CONFIG_FB_ADDR */
    #elif defined(CONFIG_VIDEO) && \
    		(!defined(CONFIG_PPC)) && \
    		!defined(CONFIG_ARM) && !defined(CONFIG_X86) && \
    		!defined(CONFIG_M68K)
    	/* reserve memory for video display (always full pages) */
    	gd->relocaddr = video_setmem(gd->relocaddr);
    	gd->fb_base = gd->relocaddr;
    #endif
    
    	return 0;
    }
    
    static int reserve_trace(void)
    {
    #ifdef CONFIG_TRACE
    	gd->relocaddr -= CONFIG_TRACE_BUFFER_SIZE;
    	gd->trace_buff = map_sysmem(gd->relocaddr, CONFIG_TRACE_BUFFER_SIZE);
    	printf("Reserving %dk for trace data at: %08lx\n",
    	      CONFIG_TRACE_BUFFER_SIZE >> 10, gd->relocaddr);
    #endif
    
    	return 0;
    }
    
    static int reserve_uboot(void)
    {
    	if (!(gd->flags & GD_FLG_SKIP_RELOC)) {
    		/*
    		 * reserve memory for U-Boot code, data & bss
    		 * round down to next 4 kB limit
    		 */
    		gd->relocaddr -= gd->mon_len;
    		gd->relocaddr &= ~(4096 - 1);
    	#if defined(CONFIG_E500) || defined(CONFIG_MIPS)
    		/* round down to next 64 kB limit so that IVPR stays aligned */
    		gd->relocaddr &= ~(65536 - 1);
    	#endif
    
    		printf("Reserving %ldk for U-Boot at: %08lx\n",
    		      gd->mon_len >> 10, gd->relocaddr);
    	}
    
    	gd->start_addr_sp = gd->relocaddr;
    
    	return 0;
    }
    
    /* reserve memory for malloc() area */
    static int reserve_malloc(void)
    {
    	gd->start_addr_sp = gd->start_addr_sp - TOTAL_MALLOC_LEN;
    	printf("Reserving %dk for malloc() at: %08lx\n",
    	      TOTAL_MALLOC_LEN >> 10, gd->start_addr_sp);
    	return 0;
    }
    
    /* (permanently) allocate a Board Info struct */
    static int reserve_board(void)
    {
    	if (!gd->bd) {
    		gd->start_addr_sp -= sizeof(bd_t);
    		gd->bd = (bd_t *)map_sysmem(gd->start_addr_sp, sizeof(bd_t));
    		memset(gd->bd, '\0', sizeof(bd_t));
    		printf("Reserving %zu Bytes for Board Info at: %08lx\n",
    		      sizeof(bd_t), gd->start_addr_sp);
    	}
    	return 0;
    }
    
    static int setup_machine(void)
    {
    #ifdef CONFIG_MACH_TYPE
    	gd->bd->bi_arch_number = CONFIG_MACH_TYPE; /* board id for Linux */
    #endif
    	return 0;
    }
    
    static int reserve_global_data(void)
    {
    	gd->start_addr_sp -= sizeof(gd_t);
    	gd->new_gd = (gd_t *)map_sysmem(gd->start_addr_sp, sizeof(gd_t));
    	printf("Reserving %zu Bytes for Global Data at: %08lx\n",
    	      sizeof(gd_t), gd->start_addr_sp);
    	return 0;
    }
    
    static int reserve_fdt(void)
    {
    #ifndef CONFIG_OF_EMBED
    	/*
    	 * If the device tree is sitting immediately above our image then we
    	 * must relocate it. If it is embedded in the data section, then it
    	 * will be relocated with other data.
    	 */
    	if (gd->fdt_blob) {
    		gd->fdt_size = ALIGN(fdt_totalsize(gd->fdt_blob) + 0x1000, 32);
    
    		gd->start_addr_sp -= gd->fdt_size;
    		gd->new_fdt = map_sysmem(gd->start_addr_sp, gd->fdt_size);
    		printf("Reserving %lu Bytes for FDT at: %08lx\n",
    		      gd->fdt_size, gd->start_addr_sp);
    	}
    #endif
    
    	return 0;
    }
    
    static int reserve_bootstage(void)
    {
    #ifdef CONFIG_BOOTSTAGE
    	int size = bootstage_get_size();
    
    	gd->start_addr_sp -= size;
    	gd->new_bootstage = map_sysmem(gd->start_addr_sp, size);
    	printf("Reserving %#x Bytes for bootstage at: %08lx\n", size,
    	      gd->start_addr_sp);
    #endif
    
    	return 0;
    }
    
    __weak int arch_reserve_stacks(void)
    {
    	return 0;
    }
    
    static int reserve_stacks(void)
    {
    	/* make stack pointer 16-byte aligned */
    	gd->start_addr_sp -= 16;
    	gd->start_addr_sp &= ~0xf;
    
    	/*
    	 * let the architecture-specific code tailor gd->start_addr_sp and
    	 * gd->irq_sp
    	 */
    	return arch_reserve_stacks();
    }
    
    static int reserve_bloblist(void)
    {
    #ifdef CONFIG_BLOBLIST
    	gd->start_addr_sp -= CONFIG_BLOBLIST_SIZE;
    	gd->new_bloblist = map_sysmem(gd->start_addr_sp, CONFIG_BLOBLIST_SIZE);
    #endif
    
    	return 0;
    }
    
    static int display_new_sp(void)
    {
    	printf("New Stack Pointer is: %08lx\n", gd->start_addr_sp);
    
    	return 0;
    }
    
    #if defined(CONFIG_M68K) || defined(CONFIG_MIPS) || defined(CONFIG_PPC) || \
    	defined(CONFIG_SH)
    static int setup_board_part1(void)
    {
    	bd_t *bd = gd->bd;
    
    	/*
    	 * Save local variables to board info struct
    	 */
    	bd->bi_memstart = CONFIG_SYS_SDRAM_BASE;	/* start of memory */
    	bd->bi_memsize = gd->ram_size;			/* size in bytes */
    
    #ifdef CONFIG_SYS_SRAM_BASE
    	bd->bi_sramstart = CONFIG_SYS_SRAM_BASE;	/* start of SRAM */
    	bd->bi_sramsize = CONFIG_SYS_SRAM_SIZE;		/* size  of SRAM */
    #endif
    
    #if defined(CONFIG_E500) || defined(CONFIG_MPC86xx)
    	bd->bi_immr_base = CONFIG_SYS_IMMR;	/* base  of IMMR register     */
    #endif
    #if defined(CONFIG_M68K)
    	bd->bi_mbar_base = CONFIG_SYS_MBAR;	/* base of internal registers */
    #endif
    #if defined(CONFIG_MPC83xx)
    	bd->bi_immrbar = CONFIG_SYS_IMMR;
    #endif
    
    	return 0;
    }
    #endif
    
    #if defined(CONFIG_PPC) || defined(CONFIG_M68K)
    static int setup_board_part2(void)
    {
    	bd_t *bd = gd->bd;
    
    	bd->bi_intfreq = gd->cpu_clk;	/* Internal Freq, in Hz */
    	bd->bi_busfreq = gd->bus_clk;	/* Bus Freq,      in Hz */
    #if defined(CONFIG_CPM2)
    	bd->bi_cpmfreq = gd->arch.cpm_clk;
    	bd->bi_brgfreq = gd->arch.brg_clk;
    	bd->bi_sccfreq = gd->arch.scc_clk;
    	bd->bi_vco = gd->arch.vco_out;
    #endif /* CONFIG_CPM2 */
    #if defined(CONFIG_M68K) && defined(CONFIG_PCI)
    	bd->bi_pcifreq = gd->pci_clk;
    #endif
    #if defined(CONFIG_EXTRA_CLOCK)
    	bd->bi_inpfreq = gd->arch.inp_clk;	/* input Freq in Hz */
    	bd->bi_vcofreq = gd->arch.vco_clk;	/* vco Freq in Hz */
    	bd->bi_flbfreq = gd->arch.flb_clk;	/* flexbus Freq in Hz */
    #endif
    
    	return 0;
    }
    #endif
    
    #ifdef CONFIG_POST
    static int init_post(void)
    {
    	post_bootmode_init();
    	post_run(NULL, POST_ROM | post_bootmode_get(0));
    
    	return 0;
    }
    #endif
    
    static int reloc_fdt(void)
    {
    #ifndef CONFIG_OF_EMBED
    	if (gd->flags & GD_FLG_SKIP_RELOC)
    		return 0;
    	if (gd->new_fdt) {
    		memcpy(gd->new_fdt, gd->fdt_blob, gd->fdt_size);
    		gd->fdt_blob = gd->new_fdt;
    	}
    #endif
    
    	return 0;
    }
    
    static int reloc_bootstage(void)
    {
    #ifdef CONFIG_BOOTSTAGE
    	if (gd->flags & GD_FLG_SKIP_RELOC)
    		return 0;
    	if (gd->new_bootstage) {
    		int size = bootstage_get_size();
    
    		printf("Copying bootstage from %p to %p, size %x\n",
    		      gd->bootstage, gd->new_bootstage, size);
    		memcpy(gd->new_bootstage, gd->bootstage, size);
    		gd->bootstage = gd->new_bootstage;
    	}
    #endif
    
    	return 0;
    }
    
    static int reloc_bloblist(void)
    {
    #ifdef CONFIG_BLOBLIST
    	if (gd->flags & GD_FLG_SKIP_RELOC)
    		return 0;
    	if (gd->new_bloblist) {
    		int size = CONFIG_BLOBLIST_SIZE;
    
    		printf("Copying bloblist from %p to %p, size %x\n",
    		      gd->bloblist, gd->new_bloblist, size);
    		memcpy(gd->new_bloblist, gd->bloblist, size);
    		gd->bloblist = gd->new_bloblist;
    	}
    #endif
    
    	return 0;
    }
    
    static int setup_reloc(void)
    {
    	if (gd->flags & GD_FLG_SKIP_RELOC) {
    		printf("Skipping relocation due to flag\n");
    		return 0;
    	}
    
    #ifdef CONFIG_SYS_TEXT_BASE
    #ifdef ARM
    	gd->reloc_off = gd->relocaddr - (unsigned long)__image_copy_start;
    #elif defined(CONFIG_M68K)
    	/*
    	 * On all ColdFire arch cpu, monitor code starts always
    	 * just after the default vector table location, so at 0x400
    	 */
    	gd->reloc_off = gd->relocaddr - (CONFIG_SYS_TEXT_BASE + 0x400);
    #else
    	gd->reloc_off = gd->relocaddr - CONFIG_SYS_TEXT_BASE;
    #endif
    #endif
    	memcpy(gd->new_gd, (char *)gd, sizeof(gd_t));
    
    	printf("Relocation Offset is: %08lx\n", gd->reloc_off);
    	printf("Relocating to %08lx, new gd at %08lx, sp at %08lx\n",
    	      gd->relocaddr, (ulong)map_to_sysmem(gd->new_gd),
    	      gd->start_addr_sp);
    
    	return 0;
    }
    
    #ifdef CONFIG_OF_BOARD_FIXUP
    static int fix_fdt(void)
    {
    	return board_fix_fdt((void *)gd->fdt_blob);
    }
    #endif
    
    /* ARM calls relocate_code from its crt0.S */
    #if !defined(CONFIG_ARM) && !defined(CONFIG_SANDBOX) && \
    		!CONFIG_IS_ENABLED(X86_64)
    
    static int jump_to_copy(void)
    {
    	if (gd->flags & GD_FLG_SKIP_RELOC)
    		return 0;
    	/*
    	 * x86 is special, but in a nice way. It uses a trampoline which
    	 * enables the dcache if possible.
    	 *
    	 * For now, other archs use relocate_code(), which is implemented
    	 * similarly for all archs. When we do generic relocation, hopefully
    	 * we can make all archs enable the dcache prior to relocation.
    	 */
    #if defined(CONFIG_X86) || defined(CONFIG_ARC)
    	/*
    	 * SDRAM and console are now initialised. The final stack can now
    	 * be setup in SDRAM. Code execution will continue in Flash, but
    	 * with the stack in SDRAM and Global Data in temporary memory
    	 * (CPU cache)
    	 */
    	arch_setup_gd(gd->new_gd);
    	board_init_f_r_trampoline(gd->start_addr_sp);
    #else
    	relocate_code(gd->start_addr_sp, gd->new_gd, gd->relocaddr);
    #endif
    
    	return 0;
    }
    #endif
    
    /* Record the board_init_f() bootstage (after arch_cpu_init()) */
    static int initf_bootstage(void)
    {
    	bool from_spl = IS_ENABLED(CONFIG_SPL_BOOTSTAGE) &&
    			IS_ENABLED(CONFIG_BOOTSTAGE_STASH);
    	int ret;
    
    	ret = bootstage_init(!from_spl);
    	if (ret)
    		return ret;
    	if (from_spl) {
    		const void *stash = map_sysmem(CONFIG_BOOTSTAGE_STASH_ADDR,
    					       CONFIG_BOOTSTAGE_STASH_SIZE);
    
    		ret = bootstage_unstash(stash, CONFIG_BOOTSTAGE_STASH_SIZE);
    		if (ret && ret != -ENOENT) {
    			printf("Failed to unstash bootstage: err=%d\n", ret);
    			return ret;
    		}
    	}
    
    	bootstage_mark_name(BOOTSTAGE_ID_START_UBOOT_F, "board_init_f");
    
    	return 0;
    }
    
    static int initf_console_record(void)
    {
    #if defined(CONFIG_CONSOLE_RECORD) && CONFIG_VAL(SYS_MALLOC_F_LEN)
    	return console_record_init();
    #else
    	return 0;
    #endif
    }
    
    static int initf_dm(void)
    {
    #if defined(CONFIG_DM) && CONFIG_VAL(SYS_MALLOC_F_LEN)
    	int ret;
    
    	bootstage_start(BOOTSTATE_ID_ACCUM_DM_F, "dm_f");
    	ret = dm_init_and_scan(true);
    	bootstage_accum(BOOTSTATE_ID_ACCUM_DM_F);
    	if (ret)
    		return ret;
    #endif
    #ifdef CONFIG_TIMER_EARLY
    	ret = dm_timer_init();
    	if (ret)
    		return ret;
    #endif
    
    	return 0;
    }
    
    /* Architecture-specific memory reservation */
    __weak int reserve_arch(void)
    {
    	return 0;
    }
    
    __weak int arch_cpu_init_dm(void)
    {
    	return 0;
    }
    
    static const init_fnc_t init_sequence_f[] = {
    	setup_mon_len,
    #ifdef CONFIG_OF_CONTROL
    	fdtdec_setup,
    #endif
    #ifdef CONFIG_TRACE
    	trace_early_init,
    #endif
    	initf_malloc,
    	log_init,
    	initf_bootstage,	/* uses its own timer, so does not need DM */
    #ifdef CONFIG_BLOBLIST
    	bloblist_init,
    #endif
    	setup_spl_handoff,
    	initf_console_record,
    #if defined(CONFIG_HAVE_FSP)
    	arch_fsp_init,
    #endif
    	arch_cpu_init,		/* basic arch cpu dependent setup */
    	mach_cpu_init,		/* SoC/machine dependent CPU setup */
    	initf_dm,
    	arch_cpu_init_dm,
    #if defined(CONFIG_BOARD_EARLY_INIT_F)
    	board_early_init_f,
    #endif
    #if defined(CONFIG_PPC) || defined(CONFIG_SYS_FSL_CLK) || defined(CONFIG_M68K)
    	/* get CPU and bus clocks according to the environment variable */
    	get_clocks,		/* get CPU and bus clocks (etc.) */
    #endif
    #if !defined(CONFIG_M68K)
    	timer_init,		/* initialize timer */
    #endif
    #if defined(CONFIG_BOARD_POSTCLK_INIT)
    	board_postclk_init,
    #endif
    	env_init,		/* initialize environment */
    	init_baud_rate,		/* initialze baudrate settings */
    	serial_init,		/* serial communications setup */
    	console_init_f,		/* stage 1 init of console */
    	display_options,	/* say that we are here */
    	display_text_info,	/* show printfging info if required */
    #if defined(CONFIG_PPC) || defined(CONFIG_SH) || defined(CONFIG_X86)
    	checkcpu,
    #endif
    #if defined(CONFIG_SYSRESET)
    	print_resetinfo,
    #endif
    #if defined(CONFIG_DISPLAY_CPUINFO)
    	print_cpuinfo,		/* display cpu info (and speed) */
    #endif
    #if defined(CONFIG_DTB_RESELECT)
    	embedded_dtb_select,
    #endif
    #if defined(CONFIG_DISPLAY_BOARDINFO)
    	show_board_info,
    #endif
    	INIT_FUNC_WATCHDOG_INIT
    #if defined(CONFIG_MISC_INIT_F)
    	misc_init_f,
    #endif
    	INIT_FUNC_WATCHDOG_RESET
    #if defined(CONFIG_SYS_I2C)
    	init_func_i2c,
    #endif
    #if defined(CONFIG_VID) && !defined(CONFIG_SPL)
    	init_func_vid,
    #endif
    	announce_dram_init,
    	dram_init,		/* configure available RAM banks */
    #ifdef CONFIG_POST
    	post_init_f,
    #endif
    	INIT_FUNC_WATCHDOG_RESET
    #if defined(CONFIG_SYS_DRAM_TEST)
    	testdram,
    #endif /* CONFIG_SYS_DRAM_TEST */
    	INIT_FUNC_WATCHDOG_RESET
    
    #ifdef CONFIG_POST
    	init_post,
    #endif
    	INIT_FUNC_WATCHDOG_RESET
    	/*
    	 * Now that we have DRAM mapped and working, we can
    	 * relocate the code and continue running from DRAM.
    	 *
    	 * Reserve memory at end of RAM for (top down in that order):
    	 *  - area that won't get touched by U-Boot and Linux (optional)
    	 *  - kernel log buffer
    	 *  - protected RAM
    	 *  - LCD framebuffer
    	 *  - monitor code
    	 *  - board info struct
    	 */
    	setup_dest_addr,
    #ifdef CONFIG_PRAM
    	reserve_pram,
    #endif
    	reserve_round_4k,
    #ifdef CONFIG_ARM
    	reserve_mmu,
    #endif
    	reserve_video,
    	reserve_trace,
    	reserve_uboot,
    	reserve_malloc,
    	reserve_board,
    	setup_machine,
    	reserve_global_data,
    	reserve_fdt,
    	reserve_bootstage,
    	reserve_bloblist,
    	reserve_arch,
    	reserve_stacks,
    	dram_init_banksize,
    	show_dram_config,
    #if defined(CONFIG_M68K) || defined(CONFIG_MIPS) || defined(CONFIG_PPC) || \
    	defined(CONFIG_SH)
    	setup_board_part1,
    #endif
    #if defined(CONFIG_PPC) || defined(CONFIG_M68K)
    	INIT_FUNC_WATCHDOG_RESET
    	setup_board_part2,
    #endif
    	display_new_sp,
    #ifdef CONFIG_OF_BOARD_FIXUP
    	fix_fdt,
    #endif
    	INIT_FUNC_WATCHDOG_RESET
    	reloc_fdt,
    	reloc_bootstage,
    	reloc_bloblist,
    	setup_reloc,
    #if defined(CONFIG_X86) || defined(CONFIG_ARC)
    	copy_uboot_to_ram,
    	do_elf_reloc_fixups,
    	clear_bss,
    #endif
    #if defined(CONFIG_XTENSA)
    	clear_bss,
    #endif
    #if !defined(CONFIG_ARM) && !defined(CONFIG_SANDBOX) && \
    		!CONFIG_IS_ENABLED(X86_64)
    	jump_to_copy,
    #endif
    	NULL,
    };
    
    void board_init_f(ulong boot_flags)
    {
    	gd->flags = boot_flags;
    	gd->have_console = 0;
    
    	if (initcall_run_list(init_sequence_f))
    		hang();
    
    #if !defined(CONFIG_ARM) && !defined(CONFIG_SANDBOX) && \
    		!defined(CONFIG_EFI_APP) && !CONFIG_IS_ENABLED(X86_64) && \
    		!defined(CONFIG_ARC)
    	/* NOTREACHED - jump_to_copy() does not return */
    	hang();
    #endif
    }
    
    #if defined(CONFIG_X86) || defined(CONFIG_ARC)
    /*
     * For now this code is only used on x86.
     *
     * init_sequence_f_r is the list of init functions which are run when
     * U-Boot is executing from Flash with a semi-limited 'C' environment.
     * The following limitations must be considered when implementing an
     * '_f_r' function:
     *  - 'static' variables are read-only
     *  - Global Data (gd->xxx) is read/write
     *
     * The '_f_r' sequence must, as a minimum, copy U-Boot to RAM (if
     * supported).  It _should_, if possible, copy global data to RAM and
     * initialise the CPU caches (to speed up the relocation process)
     *
     * NOTE: At present only x86 uses this route, but it is intended that
     * all archs will move to this when generic relocation is implemented.
     */
    static const init_fnc_t init_sequence_f_r[] = {
    #if !CONFIG_IS_ENABLED(X86_64)
    	init_cache_f_r,
    #endif
    
    	NULL,
    };
    
    void board_init_f_r(void)
    {
    	if (initcall_run_list(init_sequence_f_r))
    		hang();
    
    	/*
    	 * The pre-relocation drivers may be using memory that has now gone
    	 * away. Mark serial as unavailable - this will fall back to the printf
    	 * UART if available.
    	 *
    	 * Do the same with log drivers since the memory may not be available.
    	 */
    	gd->flags &= ~(GD_FLG_SERIAL_READY | GD_FLG_LOG_READY);
    #ifdef CONFIG_TIMER
    	gd->timer = NULL;
    #endif
    
    	/*
    	 * U-Boot has been copied into SDRAM, the BSS has been cleared etc.
    	 * Transfer execution from Flash to RAM by calculating the address
    	 * of the in-RAM copy of board_init_r() and calling it
    	 */
    	(board_init_r + gd->reloc_off)((gd_t *)gd, gd->relocaddr);
    
    	/* NOTREACHED - board_init_r() does not return */
    	hang();
    }
    #endif /* CONFIG_X86 */

    BR Rio

  • Hi Rio, 

    The patch I posted is to facilitate early UART print in SPL before normal SPL banner serial output.

    The file you attached (/common/board_f.c) is to be built into u-boot, where printf(), debug()… can be used normally w/o my patch. 

    Best,

    -Hong