Part Number: AM3352
Tool/software: TI C/C++ Compiler
Hi
Our testing department has detected the following problems:
The CPU of our board is am3352. There is an OTG interface on the board. The driver of OTG is g_ mass_ storage.
When OTG is used as a slave, it is connected to a PC, and the system of PC is win10.
When we safely remove the OTG device, we connect it to the PC again. The PC cannot recognize the OTG slave device.
The version of the SDK we use is: 05.03.00.07