This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Facing Issue when 12Tx is Enabled

Hi,

When 12 Tx is enabled using the config files or by modifying the code in chains_common_cascade_ar12xx_config_mimo.c,

I'm facing the following issue while executing the Object Detection usecase:

[ 164.773198] ------------[ cut here ]------------
[ 164.777853] WARNING: CPU: 0 PID: 0 at drivers/bus/omap_l3_noc.c:147 l3_inter0
[ 164.787028] 44000000.ocp:L3 Custom Error: MASTER DSP1_CFG TARGET EVE2 (Idle)s
[ 164.798554] Modules linked in: memcache(O) usb_f_ecm g_ether usb_f_rndis u_el
[ 164.837636] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 4.19.71
[ 164.845063] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 164.851182] Backtrace:

while 10Tx case works perfectly.

Processor SDK vision used is v3.8.

Any help would be appreciated.

Thanks,

Sowmya N