This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455 SRIO Direct IO error



I got much help from the forum and this is the first time to post a message, wish your help, my dear friends.

 

I use SRIO NWRITE_R mode to write data to 6455 Dsp0 L2 RAM from 6455 Dsp1.

different destination address LSB (the left column) and diffrent byte count (the first row), with the results (S-success, F-fail):

            1          2          3           4          5          6          7          8         9+ (bytes)

0         S          S          S          S          S          S          S          S         S

1         S           F         F          F          F          F          S          S         S

2         S          S          F          F          F          S          S          S         S

3         S          F          F          F          S          S          S          S         S

4         S          S          F          S          S          S          S          S         S

5         S          F          S          S          S          S          S          S         S

6         S          S          S          S          S          S          S          S         S

7         S          S          S          S          S          S          S          S         S

When failed, the error code is: 100b-Transaction complete, packet not sent due to unsupported transaction type or invalid programming encoding for one or more LSU register field (from spru976)

Can any one show me the reason? Thanks!