Other Parts Discussed in Thread: DM3730
I would like to know about SmartReflex on DM3730EVM.
Is SmartReflex supported CPU clock; 1GHz?
Because the error message was appeared on the following setting.
- CPU clock of DM3730EVM is 1GHz.
- SmartReflex of VDD1 is enable.
# echo 1> /sys/power/sr_vdd1_autocomp
OPP4 doesn't support SmartReflex
When CPU clock is 800MHz, there was no error message.
And the SmartReflex of VDD1 could be enable.
If it supports CPU clock; 1GHz, how does it change the setting
to be enable SmartReflex?
Regards,
Kanae