This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5749: Swap file



Hello support!!!

I use ti-processor-sdk-linux-am57xx-evm-06.03.00.106 on am5749 (custom board).

After run Linux on my board  I use: cat /proc/meminfo

I see:

SwapTotal:             0 kB
SwapFree:              0 kB

Is it normal ?

  • Hi Oleg,

    Yes even i am observing the same:

    cat /proc/meminfo | grep Swap
    SwapCached:            0 kB
    SwapTotal:             0 kB
    SwapFree:              0 kB
    root@am57xx-evm:~# free -k                      
                  total        used        free      shared  buff/cache   available
    Mem:        1636252      127268     1334608       18608      174376     1467176
    Swap:             0           0           0

    If you need to add may be you can try:

    Best Regards,
    Keerthy