Part Number: TDA4VM
Dear TI ,0211.error.txt
I have Ethernet link down error on EVM which i never had on EVM while trying to boot u-boot from OSPI and rootfs from eMMC.
SDK used is 07_00_00
Attached is the error.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Dear TI ,0211.error.txt
I have Ethernet link down error on EVM which i never had on EVM while trying to boot u-boot from OSPI and rootfs from eMMC.
SDK used is 07_00_00
Attached is the error.
Hi Manish,
"I have Ethernet link down error on EVM which i never had on EVM while trying to boot u-boot from OSPI and rootfs from eMMC."
Did you mean you never saw that on EVM and you are seeing that on custom board? Can you please explain?
Or you meant you never were successful with ethernet connection?
Please give more details.
Best Regards,
Keerthy
Hi Keerthy,
The error comes on the EVM and I never had that sort of error on EVM. We had that sort of error on our custom board but that had to do with our external broadcom switch configuration.
When i set the bootargs as you can also see in the text file to boot the rootfs from eMMC than it get stucks at 5.00 something with Ethernet error.
Regards
Manish
Hi Manish,
Help me understand what change is causing this behavior on EVM? eMMC boot is always causing this?
Best Regards,
Keerthy