This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: maxpooling problem

Part Number: TDA4VM


Dear TI,

when I use a maxpooling with kernel size = 3X3 , stride = 1, padding = 1, and the maxpooling's input is all negative, but it's output is all zero.why?

  • Only border outputs are expected to be zero.

    Can you share the SDK version and Model that you are using to reproduce the issue

  • the version is psdk_rtos_auto_j7_07_00_00_11,and my onnx model is here. The maxpooling's output is all zero.

  • This is my onnx model file.efficientdet.zip

    And this is my tidl imported model.efficientdet_tidl.zip

    This is my import config file.

    modelType = 2
    numFrames = 1
    numParamBits  = 16
    numFeatureBits = 16
    quantizationStyle = 3
    inputNetFile       = "../../test/testvecs/models/public/onnx/efficientdet/efficientdet.onnx"
    outputNetFile      = "../../test/testvecs/config/tidl_models/onnx/efficientdet.bin"
    outputParamsFile   = "../../test/testvecs/config/tidl_models/onnx/efficientdet_"
    inWidth  = 1024
    inHeight = 512
    inNumChannels = 3
    inDataFormat = 0
    inData = ../../test/testvecs/config/1024.txt
    postProcType = 0
    inDataNorm = 1
    inMean = 0 0 0
    inScale =  1 1 1
    debugTraceLevel = 1
    writeTraceLevel = 3
    foldPreBnConv2D = 0
    foldBnInConv2D = 1
    outDataNamesList = "963,962,959,output"
    

  • thanks, that's my own code problem.

  • But the maxpooling method is different from pytorch. And when the input has many negative inputs and has padding, the output also has some problems. It will generate many zeros.   

  • Hi,
        Is this issue still open?

    Regards,

    Anshu