Hello Support!!
I have the similar problem like in my post about Kernel is here: e2e.ti.com/.../3436824
I would like to use cross compilation on my host machine based on Ubuntu 18.04. I use ti-processor-sdk-linux-am57xx-evm-06.03.00.106
My compiller is : arm-linux-gnueabihf-gcc-8 (Ubuntu/Linaro 8.4.0-1ubuntu1~18.04) 8.4.0
Copyright (C) 2018 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
I change a top make file in directory U-boot:
# Make variables (CC, etc...)
AS = $(CROSS_COMPILE)as
LD = $(CROSS_COMPILE)ld
CC = $(CROSS_COMPILE)gcc-8
CPP = $(CC) -E
AR = $(CROSS_COMPILE)gcc-ar-8
NM = $(CROSS_COMPILE)gcc-nm-8
I do:
1.make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- clean
2.make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- defconfig KBUILD_DEFCONFIG=am57xx_evm_defconfig
3.make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
But after that i have a error like this:
scripts/kconfig/conf --syncconfig Kconfig
CHK include/config.h
UPD include/config.h
CFG u-boot.cfg
/bin/sh: 1: arm-linux-gnueabihf-gcc: not found
scripts/Makefile.autoconf:77: recipe for target 'u-boot.cfg' failed
make[1]: *** [u-boot.cfg] Error 1
make: *** No rule to make target «include/config/auto.conf», needed by «include/config/uboot.release». Stop.
BR
Oleg