Hi TI!!!
I am new with the processors,
I have developed a custom hardware with the AM4372, in the hardware I have, SD card slot, RAM memory, IC Flash NAND eMMC memory, PHY LAN chip, another interfaces as USB, UART, GPIO, and a power manager PMIC. I have set it the sys boot pins too.
I want to run a Linux system from the image in yhe SD memory. Then my question:
Wich are the steps for run the Linux system in my custom hardware?
There are a user guide or another documentation?
How to set the PMIC for set the corrects voltage levels?
Sincerely, Thank you very much!!!
Best regards!!!