Dear TI Processor Team:
my customer has modified the CAL example CaptureCal to connect to a MIPI-CSI2 board with 4 lanes running @1.5Gbps.
When doing this he was wondering what is the role of the FVID2 driver (<ti/drv/fvid2/fvid2.h>) in this example
and in general.
Therefore my questions are:
1. What means the abbreviation FVID2 ?
2. Is there a document, e.g. functional description, about the FVID2 explaining the possibilities and the application of it ?
I´m looking forward to your quick response.
Best regards,
Joe