I was wondering if there is any documentation that specifies how to align the bus of a raw CMOS imager to the VPIF for raw data capture. The issue is that in the DM6437 series DSPs, if you want to capture 8 Bit video, data lines D2-D9 are used on the video port of the DSP, while 10 bit video uses D0-D9. I don't see anything in the OMAP/AM/C674x documentation that describes which pins are used when the VPIF is configured to capture 8 or 10 bit video; it only states that it is possible to do so.
Any help would be appreciated. Thanks.