Other Parts Discussed in Thread: AM3517
Need to add operator isolation barrier to high speed USB port. Does anyone know of any designs that provide 2.5KV isolation of the ULPI interface and allow high speed USB 2.0 operation?
Currently envisioned design using the ULPI subsystem of the AM3517 processor, parallel 150Mbps isolation barriers and SMSC USB3320 (Highly Integrated Full Featured Hi-Speed USB 2.0 ULPI Transceiver) with minimal glue logic. There are problems with the timing of control signals (most critically being the STP signal wrt CLK) due to the large propagation delays and propagation delay spread of isolators.
Any help greatly appreciated.
Regards.