Other Parts Discussed in Thread: AM1707
I am trying to sample data via McASP port with EDMA serving the McASP. Suppose the EDMA will trigger CPU interrupt. However, interrupt didn't happen. Any suggestion is appreciated.
Signal and control flows are shown below:
1. McASP0 is used to transfer data. It is set with Ping-Pong buffering format. Data are served through DMA data port. This looks working right because data change of EDMA PaRAM 0 and 1 are observed, and EDMA IPR register was set by TCC interrupt.
2. According to the default EDMA event assignment, EDMA event 0 and 1 are assigned to McASP0, EDMA channel 0 and 1 are used for serving McASP0. Ping-Pong buffers were set for both receiving and transmitting channels. TCC interrupt is enabled. Linking are properly set. Registers of EMR, QEMR, CCERR, ER, SER, IPR, QEER and QSER are cleared at EDMA3 initilization; and EER was set as 0x03 to enable EDMA event 0 and 1; IER was set as 0x18 to enable TCC interrupt because the TCCs are set as 3 & 4. (Note: All above registers are EDMA3CC registers, not Shadow Region n Channel Registers). It looks working fine because the IPR register was set to 0x18 by the TCC interrupts. However, CPU interrupt didn't happen. CPU IFR keeps as 0.
3. CPU interrupt was enabled by setting ISTP to interrupt _vectors, CPU IER registers is set as 0x0103 to enable INT8; and CSR->GIE bit is set to 1. But CPU IFR never changed (kept as 0), and interrupt didn't happen.
4. Because the CPU INT8 event is EDMA3_CC0_INT1 as default, I set EDMA3 DRAE1 as 0x3 to enable EDMA3 event 0 and 1; then set EDMA3 Shadow Region 1 Channel Registers by clearing ER, SE, IPR, QEER and QSER, and set EER to 0x3 to enable EDMA3 event 0 and 1; IER as 0x18 to enable TCC interrupt. However, IER cannot set, it keeps 0 after write 0x18 into IESR. IPR was never changed by TCC interrupt. (Note: here all EDMA3 register are refered as Shadow Region 1 Channel Registers.)
After added this setting change, CPU interrupt was the same as before, IFR keeps as 0.
It looks like something is wrong between the EDMA3 interrupt to CPU interrupt, maybe the Interrupt Controller. My questions related to above are:
A. Is it necessary to set (enable) EDMA3 Shadow Region to enable EDMA3 triggering CPU interrupt? or it is enough to just use EDMA3 Channel Control Registers to have CPU interrupt?
B. Why IER in EDMA3 Shadow Region n Channel Registers cannot be set?
C. What is wrong with my setting which CPU interrupt doesn't happen? Specially, what is wrong with the Interrupt Controller ?
D. I checked the CPU interrupt event has EDMA3_CC0_INT1 assigned to #8, but I didn't find EDMA3_CC0_INT0 assigned to any number; which means EDMA3_CC0_INT0 cannot trigger CPU interrupt. Why did it designe this way?