Other Parts Discussed in Thread: TPS65950, DM3730
Hi,
I am designing a board with DM3730 (CBP package) and power companion TPS65950.
When I look at some design references I keep seeing that DM3730 pin AG20 (VDDS) is connected to TPS65950 pin B2 (VCCAUX4). I know that this same pin AG20 was formerly used as VDDS_CSI2 in previous generations of the OMAP processor. However the latest DM3730 datasheet says that pin AG20 is a regular vdds pin.
My question is; can I safely connect pin AG20 to regular 1.8V?
I would like to avoid the VCCAUX4 connection if possible. This way I wouldn't need to put the 1uF capacitor on VAUX4.OUT because I wouldn't be using it.
Thanks.