art Number: TDA2SX
Hi,
My requirement is 1920*1080P、30fps、3ch(VIP2 S2 A、VIP3 S1 A、VIP3 S2 A)
SDK : PROCESSOR_SDK_VISION_03_05_00_00
usecase : Chains_lvdsVipMultiCam_Display
decoder : techpoint TP2824 * 2
Q1:
How to set in the orange box in the second picture below
For example, if I use 25fps, do I need to modify the fps parameter?
Q2:
I have seen channel 2(vout 6) but other channels only have black screens
First, I modified the PINMUX and Capture parameters as shown below:
C:\PROCESSOR_SDK_VISION_03_05_00_00\ti_components\drivers\pdk_01_10_01_06\packages\ti\drv\vps\src\boards\src\bsp_boardTda2xx.c
And then i modify the VidSensor_CreateParams below:
Capture link can capture 30 frame