I can see there's a 9 port Gb switch with the port facing the CPU referred to as "CPPI".
Is this port limited to 1Gb speed or can it run faster? For example, if 2 or more external ports are receiving 1Gb/sec traffic destined for the CPPI port - can this performance be maintained or will the switch start blocking as it can't maintain throughput?
We would like to be able to sustain 3-4 ports receiving at 1Gb/s & save this data to NVMe/PCIe SSD