Other Parts Discussed in Thread: OMAPL138
Hi
I am just wondering whether the dsplink (dsplink_1_65_00_02) have support for CONFIG_PREEMPT_RT version of linux kernel.
I got OMAPl138 EVM board and is able to run the hello_world_dsp programe with default TI DVSDK linux-2.6.33-rc4-psp03.20.00.13 kernel and dsplink_1_65_00_02.
When I compiled the closest linux kernel 2.6.33.7 with CONGOG_PREEMPT_RT patch (rt30), and recompiled all the c6run and dsplink_1_65_00_02 against this new kernel, the hello_world_dsp programme hangs the system
Both cmem.ko and dsplinkk.ko driver load is successful in the COFIG_PREEMPT_RT kernel, also the hello_world_arm works fine(no surprise).
It looks to me dsplink driver is not fully complaint with CONFIG_PREEMPT_RT kernel, or am I missing something here.
Any help or pointers is highly appreciated.
Thanks,
Shameer