Advice please where can I get ONLY source codes of the kernel 2.6.29-rc3-omap1.
I not need a not a full DVSDK package, nor a latest verson.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Advice please where can I get ONLY source codes of the kernel 2.6.29-rc3-omap1.
I not need a not a full DVSDK package, nor a latest verson.
Hi Vadim,
Below mentioned is the path for downloading 2.6.29-rc3.
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_3_00/3_00_00_40/index_FDS.html
You can donwload the OMAP35x_PSP_SDK_setuplinux_02.01.02.09.bin
Hope this helps
Regards,
N.S.SriHarsha
Also you can directly down load code from Arago repository -
http://arago-project.org/git/projects/?p=linux-omap3.git;a=shortlog;h=refs/heads/OMAPPSP.02.01.03.11
Thanks,
Vaibhav